This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

make oldconfig problem

Hi,

I'm trying to add some kernel features to the am335x_evm_defconfig. so when I try these cmds :

make ARCH=arm CROSS_COMPILE=arm-eabi- am335x_evm_android_defconfig
make oldconfig or make oldconfig ARCH=arm CROSS_COMPILE=arm-eabi

I get a lot of weird question like one concerning the processor family and with no ARM entry as an
answer.
In the other hand, when I try to enable the new kernel features that I want through the
make menuconfig command, I get the same wierd questions when I run this command:
make ARCH=arm CROSS_COMPILE=arm-eabi- uImage

and it says

scripts/kconfig/conf --silentoldconfig Kconfig
*
* Restart config...
*
*
* Linux/arm 3.2.0 Kernel Configuration
*

 So, I'm guessing that there some trick that I can't figure out.


I appreciate any help.
Thanks in advance.

B.R
command,
  • Hello,

    I would recommend these steps to build the kernel and configure it:

     

    make ARCH=arm CROSS_COMPILE=arm-eabi- mrproper

    make ARCH=arm CROSS_COMPILE=arm-eabi- am335x_evm_android_defconfig

    make ARCH=arm CROSS_COMPILE=arm-eabi- menuconfig

    make ARCH=arm CROSS_COMPILE=arm-eabi- uImage

     

    This should allow you to load the default configuration, configure it with menu config, and then build uImage.

    Regards,

    Dave