Hi,
In DM8148, the DSP can not access McBSP directly (at physical address 0x47000000), but it should go through the system MMU, which translates the physical addresses to virtual addresses.
1) How can the mmu be configured to access the McBSP registers directry from the DSP?
2) Can this configuration be done from the dsp? from the arm?
3) Is it done be programming the mmu registers or by using linux commands?
Thanks,
Gilad