This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Installing SGI EVM file system and kernel.

Hello,

I just received the SGI EVM board. I am trying to install the file system and kernel. I am following the http://processors.wiki.ti.com/index.php/SGI_EVM_Software_Manual#Setup_Filesystem instruction manual.

I am stuck on getting the SD device node. When I run dmesg I can't see any SDB nodes.

Here is the output of lsblk:

hugo@hugo-HP-ProBook-4530s:~$ lsblk
NAME        MAJ:MIN RM   SIZE RO TYPE MOUNTPOINT
sda           8:0    0 232.9G  0 disk
├─sda1        8:1    0  97.7G  0 part /
├─sda2        8:2    0   100M  0 part
├─sda3        8:3    0 132.2G  0 part
├─sda4        8:4    0     1K  0 part
└─sda5        8:5    0     3G  0 part [SWAP]
sr0          11:0    1  1024M  0 rom  
mmcblk0     179:0    0   1.9G  0 disk
├─mmcblk0p1 179:1    0  78.5M  0 part /media/hugo/START_HERE
└─mmcblk0p2 179:2    0   1.6G  0 part /media/hugo/ROOTFS

with which device should I use mksdboot script?

Thanks,


Hugo.