Hello all,
please advise me of a DSP evaluation board/module that will execute full-duplex encode and decode simultaneously. 2 ethernet ports are required on the board. I want to input raw video data from a CCD sensor and input it into one port and encode it H.264 . The output will be sent to a WIFI board. The second port on the board will input H.264 from another location through the network and decode the video for viewing at the camera. An LCD screen will be at the camera. The end result is 2-way video processing. H.264 video output is 1-10 megabits per second. The arriving video (from the network) is 1-5 megabits per second. Also I would like the evaluation board to scale the video on-the-fly before it is sent out of the board. After my development is complete, I would like to use one board with one TMS chip, 2 I/o ethernet ports to perform the decode. The 2nd board with 2 I/O ethernet ports will perform the encode. I want to download the proven software from the eval board to 2 smaller boards - as products - about the size of 50mm X 50mm -- to be installed into a product enclosure. Thanks for your help.
Corby