This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Migration to EZSDK_05.05

Hi

My custom board software is based on EZSDK 05.04.00.11.

However, EZSDK 05.04.00.11 has memory leakage problem in openmax (640 byes leaked after every media file playback).

This problem seesm to have been solved in EZSDK 05.05.

However, I do not wish to migrate my target software completely to EZSDK 05.05. Rather I wish to pick components / files that have resolved the memory leakage during media playback. Which component in EZSDK 05.04 shall I upgrade to EZSDK 05.05 version to benefit from this resolution.

My custom board is configured for 512M bytes DDR and I have configured my IPC_SR_FRAM_BUFFERS to 0xB3000000 with size 60MBytes.

  • Hi Salim,

    The have a release note showing the differences between the EZSDK OMX versions.

     ti-ezsdk_dm816x-evm_5_05_02_00/component-sources/omx_05_02_00_48/OMX_05_02_00_48_ReleaseNotes.pdf

    Following IRs are addressed in omx 05.02.00.48 release

    SDOCM00095335 - Memory leak of 128 bytes in configureUIALoggerClient

    Check the below thread for more info:

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/193848.aspx

    Regards,

    Pavel