Other Parts Discussed in Thread: LM3526
On my board i have connected USB0 as a Host. ID pin is connected directly to ground, USB0_DRVVBUS is driven enable pin of 5V power IC (LM3526M-H). USB0_VBUS is connected to the switsching Power of LM3526M-H. My problem is that there are no Power on VBUS, it is only there for 600ms, than DRVVBUS goes low and the Output of LM3526 is schwitched off. If i cut the connection of DRVVBUS to LM3526, DRVVBUS is just 100ms active, so in my opinion the VBUS pin detected something because it takes more time, but nevertheless something fails becuase DRVVBUS goes low. Has anyone an idea?
regards
Markus