This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

u-boot fail message



Hi, I test my DM8168 EVM,and set nand boot mode some message occur as follow:

U-Boot 2010.06 (Mar 20 2013 - 04:26:14)

TI8168-GP rev 1.1

ARM clk: 987MHz
DDR clk: 796MHz

I2C:   ready
DRAM:  2 GiB
NAND:  HW ECC BCH8 Selected
NEW_BUSW is:2
test program dev_id = 202
_IF FIXME busw is 2
256 MiB
MMC:   OMAP SD/MMC: 0
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
*** Warning - bad CRC or NAND, using default environment

:,;;:;:;;;;;;;;r;;:,;;:;:;;;;;;;;:,;;:;:;;;;;;;;:,;;:;:;;;;;;;;:;;;;;;;;:,;;:;:
;,;:::;;;;r;;;rssiSiS552X5252525259GX2X9hX9X9XX2325S55252i5:,;;:;:;;;;;;;;:,;;:
;:;;;;;;;rrssSsS52S22h52299GGAAMHMM#BBH#B#HMM#HMBA&&XX2255S2S5Si:,;;:;:;;;;;;;;
;:;;r;;rsrrriiXS5S329&A&MH#BMB#A&9XXA252GXiSXX39AAMMMBB&G22S5i2SSiiiisi:,;;:;:;
;;;;;r;rr2iisiih393HB#B#AA99i22irrrX3X52AGsisss2Xii2299HBMA&X2S5S5iSiisSsi:,;;:
r:r;rrsrsihXSi2&##MHB&Ahh3AGHGA9G9h&#H##@@@##MAMMXXX9SSS29&&HGGX2i5iisiiisisi:,
;;rrrrsSiiiA&ABH&A9GAGhAhBAMHA9HM@@@@@@@@@@@@@@@@@@@HHhAh2S2SX9&Gh22SSiisiiisii
r:rrssisiS2XM##&h3AGAX&3GG3Ssr5H@M#HM2; ;2X&&&MHMB###GBB#B&XXSSs529XX55iSsisisi
r;rsrisSi2XHAhX99A3XXG&&XS;:,rH#HGhAS   @@@@3rs2XBM@@A552&&AHA2XiisSS252SSsisSs
r;issi5S22&&3iSSX292&hXsr;;:;h@&G339&S9@@@@2@MA&9&HB##Xris29ABMAAX2ir;rsSi5iss5
rrsSi2XhG&9GXh399&X99i;;;;;;r#H&293H9X#@@@@@@@B&9GhAH@XrrsrsiXABHB&HG2rr;rrSiSi
;:rsisS599&AA9XG&3A35r;:::;,;BMh&&2iX5A@@@@@@@&392X5GB2;;;r;iSX393A##A&Xi:::rsi
;:rss552222X553&XHMhir;;::,:,h#HhGSXhG3#@@@@#AXXS2XAHA;::;;;;ss55XShBA3239r:,;;
r;ii2S5SSi2i53hirsh2srr::,,,,;MMXX359&Ah3h&Si59SX99A#i:,::::;;sri2,.2r;:SGAr;,:
;:;rrrrssiriXGSi::shs;;;,,,:,,rBBA9h5s5h5iS5isi2SAHB5:,,,:::;rrs5&SrisSX5Srrr:,
;,r;;;;rsriSSrrrr;;5Xrr;;,:,,.,;9AA2SsisS5323XXXG9&i:.,,::;;r;;;srrrrrr;;:;::::
:,;r;r;rrissrrr;:;::;s;;;;,:,,..,r293h222hXXAAGGGX;:,,,:,:,::;:;::,:,,,,...,,,,
;,;;;;rrrrrrrrirr;,.,,:::::::,,,,.,;SX&ABAB2hhXir:,,.,,.,,:,,,,..,,,..,..,,,..:
:.:;:;;;:;;;;r;rrs;:.. ,,:::::,:,:,,.::rrsrr;;,,.......,..,....,,,,,,,...,.,,:,
:.:::,::::::;;r;rrr;:.......,.,.,,:::,,...............,,::.,,,,:,::,,:,:,,,:,;:
,.::,:,,,,,;;;;;;;;r;;::,..............................;;;:;::::,:::::::,:,:,,,
: ,,:,,,,,,,,,,,,,:;rrr;;:;,,,,,,,::,.,.:.,.,;s,:;;;;:;:;;;;;::::,:::,:::,:,:,:
,.,,,,,,,...,,.,,....................................:,............:,,,:,:,,,,,

Net:   <ethaddr> not set. Reading from E-fuse
Detected MACID:90:d7:eb:35:9f:1c
Ethernet PHY: GENERIC @ 0x01
DaVinci EMAC
Hit any key to stop autoboot:  0
TI8168_EVM#

I use u-boot version is u-boot-2010.06-psp04.04.00.01.

But, when I use the version u-boot-2010.06-psp04.00.00.01, the ECC error can not happen. what may the problem for u-boot-2010.06-psp04.04.00.01 version? and how to solve the problem?

 

Thanks,

Chen

 

 

  • Chen,

    This could be because the previous version of the u-boot or the NAND memory area is written using a different ECC scheme.

    Please erase the complete NAND area using the following command and try flashing the u-boot image

     
    TI8168_EVM#   nand scrub