Other Parts Discussed in Thread: AM3352
Hello experts,
Is there a way to determine the speed grade of AM335x through software--perhaps by checking a register? I know of the DEVICE_ID and DEV_FEATURE registers, which do not seem to contain the needed speed grade information.
The reason I am asking this is because of the following scenario: if you have a situation where you are using the same board for two slightly different versions of a product, one of which contains a lower speed grade of AM3352 and then other with a higher speed grade AM3352, is there a way by which this difference can be determined by software without having to have use external memory or another mechanism to indicate this?
Thanks,
Josh