hi, I want to use the RS485 port in the DM365 3.0 release; but , i scan the boot message ,find only have one Serial port for console :
[ 0.200000] serial8250.0: ttyS0 at MMIO map 0x1d06000 mem 0xfbd06000 (irq = 41) is a 16550A
while,it's not happened in the 2.6 release,it have two serial port : ttyS0 and ttyS1(RS485).
this is the difference between 2.6 and 3.0 release about configuration :
Relative to the 2.6 release, anything to be change about RS485 in the 3.0 release ?
Anything I'm missing? What to try next?