Hi
I wanted to check if any of the 3 OMAP4 devices, 4430, 4460, 4470 are capable of 1080p60 decode?
If yes, what are the clock frequency settings for the various cores to be able to achieve this decode - A9, M3, IVA.
Do these clock frequencies get set automatically if 1080p60 content is being decoded or do i need to configure any of them specifically to a particular value?
I have blaze-tab 2 devices running ICS and JellyBean.
Thanks
Anoop