This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3359ICE Boot Program

Guru 15520 points
Other Parts Discussed in Thread: AM3359

Hi,

I have a question about AM3359 ICE Board.

What kind of application is contained in the NOR/SPI memory at the time of shipment?
Is both NOR and SPI flash contain pre-build LED application which are in the ISDK?

best regards,
g.f.

  • Not sure if we can give a good answer to that one... It depends on the build batch.

    It should have at least boot loader and example app in SPI (don't think we flash NOR at all...). For sure the 3P doing the production does not keep up with the IA-SDK releases so I would always recommend to flash the latest from the IA-SDK (using the binary package should give you all the files needed). That ensures you know exactly what is on the board and it is the latest version :-). This will also allow us to better answer questions. Obviously we do not want to work through fixed issues again and will ask you to test with actual versions first.

    Regards.

  • Hi, Frank

    Thank you for the answer.
    I understood.

    best regards,
    g.f.