Other Parts Discussed in Thread: TVP5150AM1, TVP5150, AM3517
Hello,
I have some problems with video device. I am using TVP5150am1 video Encoder. I want to connect to video camera (using composite inpute of TVP5150am1). But when I try to use /dev/video0 (device of encoder) V4L freeze and It does not show anything. I try to acces it with a simple code using V4L, and mplayer.
Actually I configured enconder in this way
/*
* VPFE - Video Decoder interface
*
* Based in board-am3517evm with TVP514x chipset we use TVP5150AM1
*/
#define TVP5150_STD_ALL (V4L2_STD_NTSC | V4L2_STD_PAL)
static struct v4l2_input tvp5150_inputs[] = {
{
.index = 0,
.name = "Composite",
.type = V4L2_INPUT_TYPE_CAMERA,
.std = TVP5150_STD_ALL,
},
};
static struct vpfe_route tvp5150_routes[] = {
{
.input = TVP5150_COMPOSITE0,
.output = TVP5150_NORMAL,
},
};
static struct vpfe_subdev_info vpfe_sub_devs[] = {
{
.name = "tvp5150",
.grp_id = 0,
.num_inputs = ARRAY_SIZE(tvp5150_inputs),
.inputs = tvp5150_inputs,
.routes = tvp5150_routes,
.can_route = 1,
/*.ccdc_if_params = {
.if_type = VPFE_BT656,
.hdpol = VPFE_PINPOL_POSITIVE,
.vdpol = VPFE_PINPOL_POSITIVE,
},*/
.board_info = {
I2C_BOARD_INFO("tvp5150", 0x5C),
},
},
};
static void am3517_evm_clear_vpfe_intr(int vdint)
{
unsigned int vpfe_int_clr;
vpfe_int_clr = omap_ctrl_readl(AM35XX_CONTROL_LVL_INTR_CLEAR);
switch (vdint) {
/* VD0 interrrupt */
case INT_35XX_CCDC_VD0_IRQ:
vpfe_int_clr &= ~AM35XX_VPFE_CCDC_VD0_INT_CLR;
vpfe_int_clr |= AM35XX_VPFE_CCDC_VD0_INT_CLR;
break;
/* VD1 interrrupt */
case INT_35XX_CCDC_VD1_IRQ:
vpfe_int_clr &= ~AM35XX_VPFE_CCDC_VD1_INT_CLR;
vpfe_int_clr |= AM35XX_VPFE_CCDC_VD1_INT_CLR;
break;
/* VD2 interrrupt */
case INT_35XX_CCDC_VD2_IRQ:
vpfe_int_clr &= ~AM35XX_VPFE_CCDC_VD2_INT_CLR;
vpfe_int_clr |= AM35XX_VPFE_CCDC_VD2_INT_CLR;
break;
/* Clear all interrrupts */
default:
vpfe_int_clr &= ~(AM35XX_VPFE_CCDC_VD0_INT_CLR |
AM35XX_VPFE_CCDC_VD1_INT_CLR |
AM35XX_VPFE_CCDC_VD2_INT_CLR);
vpfe_int_clr |= (AM35XX_VPFE_CCDC_VD0_INT_CLR |
AM35XX_VPFE_CCDC_VD1_INT_CLR |
AM35XX_VPFE_CCDC_VD2_INT_CLR);
break;
}
omap_ctrl_writel(vpfe_int_clr, AM35XX_CONTROL_LVL_INTR_CLEAR);
vpfe_int_clr = omap_ctrl_readl(AM35XX_CONTROL_LVL_INTR_CLEAR);
}
static struct vpfe_config vpfe_cfg = {
.num_subdevs = ARRAY_SIZE(vpfe_sub_devs),
.i2c_adapter_id = 2,
.sub_devs = vpfe_sub_devs,
.clr_intr = am3517_evm_clear_vpfe_intr,
.card_name = "DM6446 EVM",
.ccdc = "DM6446 CCDC",
};
static struct resource vpfe_resources[] = {
{
.start = INT_35XX_CCDC_VD0_IRQ,
.end = INT_35XX_CCDC_VD0_IRQ,
.flags = IORESOURCE_IRQ,
},
{
.start = INT_35XX_CCDC_VD1_IRQ,
.end = INT_35XX_CCDC_VD1_IRQ,
.flags = IORESOURCE_IRQ,
},
};
static u64 vpfe_capture_dma_mask = DMA_BIT_MASK(32);
static struct platform_device vpfe_capture_dev = {
.name = CAPTURE_DRV_NAME,
.id = -1,
.num_resources = ARRAY_SIZE(vpfe_resources),
.resource = vpfe_resources,
.dev = {
.dma_mask = &vpfe_capture_dma_mask,
.coherent_dma_mask = DMA_BIT_MASK(32),
.platform_data = &vpfe_cfg,
},
};
/* END - VPFE - Video Decoder interface */
I do not know how I am doing wrong. Suggestions?
Thanks a lot.