This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can't able to boot EVM335x rev 1.2A and 1.1 A board from SD card

I have installed AM335x-evm-SDK-bin-05.06.00.00 and try to boot pre-built MLO,Uboot, linux image(uImage) from SD card on EVM335x rev 1.2A and 1.1 A board. 

My aim is to boot it from SD card.

I prepared the Sd card 3 partition ---- did dip switch setting of evm board ------ copied MLO, uboot, UImage into boot section ---- untar rootfs into rootfs section and followed all steps till sync ----- configured serial port of PC at 115200 8N1 no flow control and connected it  to Rs232 0 of target ----- nothing appears on the screen

what I am reciving are special characters"ÁÁÁÁÁÁãÁÁÁÁÁÁÁÁãÁãáÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁãÁÁãÁÁããÁããÁÁÁáãÁãÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁÁãÁÁÁÁÁÁÁÁÁ" Or sometime "CCCCC" on console.

Please let me know where I'm wrong.