This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The connection of oscillator on TMDSSK3358

Guru 16800 points


Hi,

I'm using a TMDSSK3358 board and checking the schematic of it.
It seem that the ground pin of the oscillator (Y6) is left floating.
Should the ground pin be connected to VSS_OSC?

Thanks

Nomoto

  • If the oscillator package has ground terminals, those terminals should also be connected to the respective Kelvin ground terminals (VSS_RTC or VSS_OSC).

    The decoupling capacitor connected to the VDDS_OSC (R11)  terminal should not be connected to the GND_OSC0 net which is connected to the VSS_OSC (V11) terminal as shown in the schematic.  This capacitor should have been connected to VSS.  I will discuss this with the person that designed this board and have him document this error in his errata document.

    Regards,
    Paul