This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[ Two Mouse Cursors ] Mouse repaint problems when display rotated in "Matrix GUI" ?

When the "Matrix GUI" application is rotated to 90 using command line option "-display transformed:Rot90",  I see two mouse cursors displayed.  One cursor is non-destructive ( the repaint must be working ) and I can click on icons using it.  The second cursor is moving at 90 degrees to the first and appears to be repainting the graphics the other one just passed over.

Does anyone know a possible solution?

Is there a low level way to rotate a screen display rather than the Qt windowing system which I assume is what matrix-gui is using?

File: /etc/init.d/matrix-gui-e

#! /bin/sh

matrixgui="/usr/bin/matrix_guiE"
GUI_OPTS="-qws /usr/share/matrix/html/menu_main.html"
# -display transformed:Rot90 
MULTI_OPTS="Multi: transformed:Rot90 LinuxFb:/dev/fb0 LinuxFb:/dev/fb1"
PIDFILE="/var/run/matrix-gui-e.pid"

test -x "$matrixgui" || exit 0

#export TSLIB_TSDEVICE=/dev/input/event1
#export QWS_MOUSE_PROTO=Tslib:/dev/input/touchscreen0
export QWS_KEYBOARD="USB:/dev/input/event0 USB:/dev/input/event1"
#export QWS_MOUSE_PROTO=Auto:/dev/input/mice
export QWS_MOUSE_PROTO=Auto:/dev/input/event1

case "$1" in
  start)
#    if [ ! -f /etc/pointercal ] ; then
#        echo -n "Calibrating touchscreen (first time only)"
#        ts_calibrate
#        echo "."
#    fi

	if [ -e $PIDFILE ]; then
      PIDDIR=/proc/$(cat $PIDFILE)
      if [ -d ${PIDDIR} -a  "$(readlink -f ${PIDDIR}/exe)" = "${matrixgui}" ]; then
        echo "$DESC already started; not starting."
      else
        echo "Removing stale PID file $PIDFILE."
        rm -f $PIDFILE
      fi
    fi

    echo -n "Starting Matrix GUI application"
    start-stop-daemon --start --quiet --background --exec $matrixgui -- -display "$MULTI_OPTS" $GUI_OPTS
	pidof matrix_guiE > $PIDFILE
    echo "."
    ;;

  stop)
    echo -n "Stopping Matrix GUI application"
    start-stop-daemon --stop --quiet --exec $matrixgui
    echo "."
    ;;
  *)
    echo "Usage: /etc/init.d/matrix-gui-e {start|stop}"
    exit 1
esac

exit 0

Thanks in advance,

-Ed