This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about BOOTCOMPLETE pin and BOOTCOMPLETE register for C6657



based on tms320c6657-23.pdf, section 3.3.9, the BOOTCOMPLETE pin is a pin reflecting the BOOTCOMPLETE register. But there are two bits in BOOTCOMPLETE register, each for one corePack, while there is only 1 single BOOTCOMPLETE pin.

Is there any document on how the mapping from the two bits to the pin? Are they AND/OR of the two bits, or does it reflect only corePack0?

thanks

Weichun