Hi,
I'm using TI dm8168 board and the EZSDK version is 5.05, and I have met the above error:hub 2-0:1.0: over-current change on port 1、.
In the "DM816x EZ Software Developers Guide" say:
"This error message will be seen if the daughter board is not connected with the J5Eco EVM. In this absence of
daughter board the USB1 port is hanging this produces the above error. In case you do not want to use
daughter card you can disable the USB1 port by applying the patch provided in PSP release notes documents."
But I have not found the patch in PSP release notes document. Can you help me found the patch?
Thanks.