Other Parts Discussed in Thread: TMS320C6678
H264 High Profile Encoder (v01.00.00) on TMS320C6678 Platform
H264 Base Profile, CBR, IPPP, CAVLC, Multi Core(2 Cores)
Shyam_p1280x720_420p_8bit.yuv, YUV420, CAVLC, CBR, IPPP @ 3Mbps @ 30 frames per second
Average cycles:983MHz
notes:
Average cycles are calculated as maximum of moving average of 30 frames, multiplied with 30 to get per second Mhz.
that means: each core works in 983MHz ? or 987MHz is the number of total cycles by two cores?how to understand?
thanks