This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C55x for loop error

Hello,

I have some code

// Read in data
for(len=0;len<length;len++) {

buffer[len] = max3421_read(0, RCVFIFO) & 0xFF;
}

that compiles into asm

C$DW$L$_max3421_bulk_in_transfer$10$B, C$L37:
0025e2: 3c04 MOV #0,T0
0025e4: 08fbab_3d15 CALL max3421_read || MOV #1,T1
0025e9: 2264_19ff04 MOV T2,T0 || AND #255,T0,AC0
0025ee: c0ab MOV AC0,*AR5(AR0)
299 for(len=0;len<length;len++) {
0025f0: 4016 ADD #1,T2
0025f2: 126470 CMP T2 < T3, TC1
0025f5: 0464ea BCC C$L37,TC1

which is incorrect. The instruction MOV AC0,*AR5(AR0) is to put values into an indexed array, but the index, AR0, never increments. Do you know why?