Hi,
Board is blaze tablet.
Code is 4AI.1.7P1.
Ducati 2.1
When you open the camera application Preview, the increase in working current of 500 mA.
This may be what causes, how to optimize?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ISS subsystem and AUXCLK are gated when camera is not running. M3 clocks are also gated when no video/camera usecase is running. The clocks are activated when application starts preview and therefore working current is expected to increase.
hi,
Mayank,
Thanks for your reply.
The platform is omap4470 ,but the platform of omap4430 the increase in working current of 200 mA when open the camera application preview.
The ducati version(2.1) of the same, and the code version(4AI.1.7P1) of the same .
There can be optimized space?
Thanks
Are you testing the same camera sensor and same preview resolution on 4470 and 4430?
maybe it is the display which is drawing more power. Can you test movie playback with same video stream on both the boards and compare the current?