This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

'PVR_K: HWRecoveryReset SGX' issue on am335x evm

Other Parts Discussed in Thread: DA8XX, TPS65910

Hi all,

I am facing an issue related to SGX on am335x running android ICS.

On the boot message it shows SGX log messages, the device takes very long time to boot up and android os is getting stuck.

How can i correct this problem?

Regards,

Ebin

bootup message -

U-Boot SPL 2011.09 (Sep 07 2012 - 18:02:57)
Texas Instruments Revision detection unimplemented
OMAP SD/MMC: 0
reading u-boot.img
reading u-boot.img
U-Boot 2011.09 (Sep 07 2012 - 18:02:57)
I2C:   ready
DRAM:  512 MiB
WARNING: Caches not enabled
NAND:  HW ECC Hamming Code selected
No NAND device found!!!
0 MiB
MMC:   OMAP SD/MMC: 0
*** Warning - readenv() failed, using default environment
EVM-Configuration : Calixto-AM335x-EVM
Net:   cpsw
Hit any key to stop autoboot:  0
SD/MMC found on device 0
reading uEnv.txt
214 bytes read
Loaded environment from uEnv.txt
Importing environment from mmc ...
Running uenvcmd ...
reading uImage
3901608 bytes read
## Booting kernel from Legacy Image at 82000000 ...
   Image Name:   Linux-3.2.0-g407167a-dirty
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    3901544 Bytes = 3.7 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[    0.000000] Linux version 3.2.0-g407167a-dirty (root@ebin-desktop) (gcc version 4.4.3 (GCC) ) #1 Thu Mar 21 22:42:46 IST 2013
[    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine: am335xevm
[    0.000000] Memory policy: ECC disabled, Data cache writeback
[    0.000000] AM335X ES1.0 (sgx neon )
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 65024
[    0.000000] Kernel command line: console=ttyO0,115200n8 androidboot.console=ttyO0 mem=256M root=/dev/mmcblk0p2 rw rootfstype=ext4 rootwait init=/init ip=off
[    0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[    0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[    0.000000] Memory: 256MB = 256MB total
[    0.000000] Memory: 250840k/250840k available, 11304k reserved, 0K highmem
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xd0800000 - 0xff000000   ( 744 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)
[    0.000000]     modules : 0xbf000000 - 0xc0000000   (  16 MB)
[    0.000000]       .text : 0xc0008000 - 0xc06a7000   (6780 kB)
[    0.000000]       .init : 0xc06a7000 - 0xc0742000   ( 620 kB)
[    0.000000]       .data : 0xc0742000 - 0xc079c840   ( 363 kB)
[    0.000000]        .bss : 0xc079c864 - 0xc08cdb10   (1221 kB)
[    0.000000] NR_IRQS:396
[    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[    0.000000] Total of 128 interrupts on 1 active controller
[    0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[    0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[    0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[    0.000000] Console: colour dummy device 80x30
[    0.000152] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[    0.058929] pid_max: default: 32768 minimum: 301
[    0.059082] Security Framework initialized
[    0.059143] Mount-cache hash table entries: 512
[    0.059509] CPU: Testing write buffer coherency: ok
[    0.079437] omap_hwmod: pruss: failed to hardreset
[    0.080230] print_constraints: dummy:
[    0.080474] NET: Registered protocol family 16
[    0.081542] OMAP GPIO hardware version 0.1
[    0.082550] omap_mux_init: Add partition: #1: core, flags: 0
[    0.083740]  omap_i2c.1: alias fck already exists
[    0.084106] The board is a AM335x Calixto EVM.
[    0.084411]  da8xx_lcdc.0: alias fck already exists
[    0.084503] Setup LCD display
[    0.084503] FUNCTION: For Registering PWM backlight..
[    0.084625] function: in board-am335xevm.c tsc_init
[    0.084899]  omap_hsmmc.0: alias fck already exists
[    0.085052]  davinci-mcasp.0: alias fck already exists
[    0.085388]  omap2_mcspi.1: alias fck already exists
[    0.085510]  omap2_mcspi.2: alias fck already exists
[    0.085662]  edma.0: alias fck already exists
[    0.085662]  edma.0: alias fck already exists
[    0.085693]  edma.0: alias fck already exists
[    0.095397] bio: create slab <bio-0> at 0
[    0.096405] SCSI subsystem initialized
[    0.097259] usbcore: registered new interface driver usbfs
[    0.097381] usbcore: registered new interface driver hub
[    0.097503] usbcore: registered new device driver usb
[    0.097625] musb-ti81xx musb-ti81xx: musb0, board_mode=0x31, plat_mode=0x1
[    0.097778] musb-ti81xx musb-ti81xx: musb1, board_mode=0x31, plat_mode=0x3
[    0.109008] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[    0.109985] tps65910 1-002d: JTAGREVNUM 0x0
[    0.112152] print_constraints: VRTC:
[    0.113525] print_constraints: VIO: at 1800 mV
[    0.115753] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal
[    0.117950] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal
[    0.118865] print_constraints: VDD3: 5000 mV
[    0.120239] print_constraints: VDIG1: at 1800 mV
[    0.121582] print_constraints: VDIG2: at 1800 mV
[    0.122894] print_constraints: VPLL: at 1800 mV
[    0.124206] print_constraints: VDAC: at 1800 mV
[    0.125549] print_constraints: VAUX1: at 1800 mV
[    0.126892] print_constraints: VAUX2: at 3300 mV
[    0.128234] print_constraints: VAUX33: at 3300 mV
[    0.129547] print_constraints: VMMC: at 3300 mV
[    0.129852] tps65910 1-002d: No interrupt support, no core IRQ
[    0.130249] Advanced Linux Sound Architecture Driver Version 1.0.24.
[    0.130859] Bluetooth: Core ver 2.16
[    0.130920] NET: Registered protocol family 31
[    0.130920] Bluetooth: HCI device and connection manager initialized
[    0.130950] Bluetooth: HCI socket layer initialized
[    0.130950] Bluetooth: L2CAP socket layer initialized
[    0.130981] Bluetooth: SCO socket layer initialized
[    0.131195] Switching to clocksource gp timer
[    0.138702] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[    0.138916] musb-hdrc musb-hdrc.0: dma type: pio
[    0.139190] MUSB0 controller's USBSS revision = 4ea20800
[    0.139343] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[    0.139434] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
[    0.139587] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[    0.139587] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    0.139617] usb usb1: Product: MUSB HDRC host driver
[    0.139617] usb usb1: Manufacturer: Linux 3.2.0-g407167a-dirty musb-hcd
[    0.139617] usb usb1: SerialNumber: musb-hdrc.0
[    0.140136] hub 1-0:1.0: USB hub found
[    0.140167] hub 1-0:1.0: 1 port detected
[    0.140563] musb-hdrc musb-hdrc.0: USB Host mode controller at d083c000 using PIO, IRQ 18
[    0.140838] musb-hdrc musb-hdrc.1: dma type: pio
[    0.140991] MUSB1 controller's USBSS revision = 4ea20800
[    0.141448] musb-hdrc musb-hdrc.1: USB OTG mode controller at d083e800 using PIO, IRQ 19
[    0.141784] NET: Registered protocol family 2
[    0.141967] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.142395] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[    0.142547] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[    0.142639] TCP: Hash tables configured (established 8192 bind 8192)
[    0.142639] TCP reno registered
[    0.142669] UDP hash table entries: 256 (order: 0, 4096 bytes)
[    0.142700] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[    0.142883] NET: Registered protocol family 1
[    0.143157] RPC: Registered named UNIX socket transport module.
[    0.143157] RPC: Registered udp transport module.
[    0.143188] RPC: Registered tcp transport module.
[    0.143188] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.143432] NetWinder Floating Point Emulator V0.97 (double precision)
[    0.275543] ashmem: initialized
[    0.275787] VFS: Disk quotas dquot_6.5.2
[    0.275848] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.276763] msgmni has been set to 489
[    0.277832] io scheduler noop registered
[    0.277832] io scheduler deadline registered
[    0.277923] io scheduler cfq registered (default)
[    0.278961] da8xx_lcdc da8xx_lcdc.0: GLCD: Found TFC_S9700RTWV35TR_01B panel
[    0.288604] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[    0.979461] console [ttyO0] enabled
[    0.983642] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[    0.991333] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[    0.999023] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[    1.006683] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[    1.014343] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[    1.027954] brd: module loaded
[    1.034240] loop: module loaded
[    1.037750] i2c-core: driver [tsl2550] using legacy suspend method
[    1.044250] i2c-core: driver [tsl2550] using legacy resume method
[    1.051574] mtdoops: mtd device (mtddev=name/number) must be supplied
[    1.058471] omap2-nand driver initializing
[    1.062835] OneNAND driver initializing
[    1.067321] CAN device driver interface
[    1.071319] CAN bus driver for Bosch D_CAN controller 1.0
[    1.077209] PPP generic driver version 2.4.2
[    1.081878] PPP BSD Compression module registered
[    1.086791] PPP Deflate Compression module registered
[    1.092163] usbcore: registered new interface driver cdc_ether
[    1.098297] usbcore: registered new interface driver cdc_eem
[    1.104278] usbcore: registered new interface driver dm9601
[    1.110137] usbcore: registered new interface driver cdc_subset
[    1.116394] cdc_ncm: 04-Aug-2011
[    1.119812] usbcore: registered new interface driver cdc_ncm
[    1.125823] usbcore: registered new interface driver cdc_acm
[    1.131713] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[    1.140075] Initializing USB Mass Storage driver...
[    1.145294] usbcore: registered new interface driver usb-storage
[    1.151550] USB Mass Storage support registered.
[    1.156555] usbcore: registered new interface driver usbserial
[    1.162719] USB Serial support registered for generic
[    1.361846] usb 1-1: new high-speed USB device number 2 using musb-hdrc
[    1.502655] usb 1-1: New USB device found, idVendor=19d2, idProduct=1523
[    1.509643] usb 1-1: New USB device strings: Mfr=2, Product=1, SerialNumber=3
[    1.517120] usb 1-1: Product: T-Mobile Rocket 4G prepaid
[    1.522674] usb 1-1: Manufacturer: T-Mobile
[    1.527008] usb 1-1: SerialNumber: MF5910TMOD000000
[    1.533050] scsi0 : usb-storage 1-1:1.0
[    1.538146] usbcore: registered new interface driver usbserial_generic
[    1.544982] usbserial: USB Serial Driver core
[    1.549591] USB Serial support registered for GSM modem (1-port)
[    1.556121] usbcore: registered new interface driver option
[    1.561950] option: v0.7.2:USB Driver for GSM modems
[    1.568908]  gadget: Mass Storage Function, version: 2009/09/11
[    1.575134]  gadget: Number of LUNs=1
[    1.578948]  lun0: LUN: removable file: (no medium)
[    1.584289]  gadget: android_usb ready
[    1.588256] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[    1.593841] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
[    1.601654] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[    1.608764] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    1.616302] usb usb2: Product: MUSB HDRC host driver
[    1.621490] usb usb2: Manufacturer: Linux 3.2.0-g407167a-dirty musb-hcd
[    1.628387] usb usb2: SerialNumber: musb-hdrc.1
[    1.633605] hub 2-0:1.0: USB hub found
[    1.637542] hub 2-0:1.0: 1 port detected
[    1.642272] mousedev: PS/2 mouse device common for all mice
[    1.648925] input: ti-tsc-adcc as /devices/platform/omap/tsc/input/input0
[    1.657409] using rtc device, omap_rtc, for alarms
[    1.662322] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
[    1.669219] i2c /dev entries driver
[    1.673065] Linux video capture interface: v2.00
[    1.678009] usbcore: registered new interface driver uvcvideo
[    1.684020] USB Video Class driver (1.1.1)
[    1.690063] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[    1.696624] device-mapper: uevent: version 1.0.3
[    1.701599] device-mapper: ioctl: 4.22.0-ioctl (2011-10-19) initialised: dm-devel@redhat.com
[    1.710449] Bluetooth: HCI UART driver ver 2.2
[    1.715087] Bluetooth: HCI H4 protocol initialized
[    1.720092] Bluetooth: HCILL protocol initialized
[    1.725006] Bluetooth: Bluetooth Driver for TI WiLink - Version 1.0
[    1.733367] cpuidle: using governor ladder
[    1.737792] cpuidle: using governor menu
[    1.743896] usbcore: registered new interface driver usbhid
[    1.749725] usbhid: USB HID core driver
[    1.754272] logger: created 256K log 'log_main'
[    1.759124] logger: created 256K log 'log_events'
[    1.764160] logger: created 256K log 'log_radio'
[    1.769104] logger: created 256K log 'log_system'
[    1.774505] usbcore: registered new interface driver snd-usb-audio
[    1.782043] _regulator_get: 1-0018 supply IOVDD not found, using dummy regulator
[    1.789794] _regulator_get: 1-0018 supply DVDD not found, using dummy regulator
[    1.797485] _regulator_get: 1-0018 supply AVDD not found, using dummy regulator
[    1.805175] _regulator_get: 1-0018 supply DRVDD not found, using dummy regulator
[    1.816101] asoc: tlv320aic3x-hifi <-> davinci-mcasp.0 mapping ok
[    1.823364] ALSA device list:
[    1.826477]   #0: AM335X EVM
[    1.829467] oprofile: hardware counters not available
[    1.834777] oprofile: using timer interrupt.
[    1.839416] Netfilter messages via NETLINK v0.30.
[    1.844451] nf_conntrack version 0.5.0 (3919 buckets, 15676 max)
[    1.851043] ctnetlink v0.93: registering with nfnetlink.
[    1.856719] NF_TPROXY: Transparent proxy support initialized, version 4.1.0
[    1.863983] NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.
[    1.870391] xt_time: kernel timezone is -0000
[    1.875213] ip_tables: (C) 2000-2006 Netfilter Core Team
[    1.880981] arp_tables: (C) 2002 David S. Miller
[    1.885894] TCP cubic registered
[    1.889434] NET: Registered protocol family 10
[    1.894866] Mobile IPv6
[    1.897491] ip6_tables: (C) 2000-2006 Netfilter Core Team
[    1.903381] IPv6 over IPv4 tunneling driver
[    1.908355] NET: Registered protocol family 17
[    1.913055] NET: Registered protocol family 15
[    1.917694] can: controller area network core (rev 20090105 abi 8)
[    1.924285] NET: Registered protocol family 29
[    1.928924] can: raw protocol (rev 20090105)
[    1.933380] can: broadcast manager protocol (rev 20090105 t)
[    1.939514] Bluetooth: RFCOMM TTY layer initialized
[    1.944671] Bluetooth: RFCOMM socket layer initialized
[    1.950042] Bluetooth: RFCOMM ver 1.11
[    1.953948] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    1.959503] Bluetooth: BNEP filters: protocol multicast
[    1.964965] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[    1.971282] Registering the dns_resolver key type
[    1.976318] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[    1.984313] ThumbEE CPU extension supported.
[    1.988830] mux: Failed to setup hwmod io irq -22
[    1.994415] Power Management for AM33XX family
[    1.999267] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[    2.005950] Copied the M3 firmware to UMEM
[    2.014709] clock: disabling unused clocks to save power
[    2.022491] input: gpio-keys as /devices/platform/gpio-keys/input/input1
[    2.029876] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
[    2.039123] Waiting for root device /dev/mmcblk0p2...
[    2.083374] mmc0: host does not support reading read-only switch. assuming write-enable.
[    2.094390] mmc0: new high speed SDHC card at address 1234
[    2.100616] mmcblk0: mmc0:1234 SA08G 7.41 GiB
[    2.107513]  mmcblk0: p1 p2 p3
[    2.563110] scsi 0:0:0:0: CD-ROM            T-Mobile USB SCSI CD-ROM  0001 PQ: 0 ANSI: 0
[    2.571929] scsi 0:0:0:1: Direct-Access     T-Mobile MMC Storage      0001 PQ: 0 ANSI: 0
[    2.581848] scsi 0:0:0:0: Attached scsi generic sg0 type 5
[    2.588226] sd 0:0:0:1: Attached scsi generic sg1 type 0
[    2.595245] sd 0:0:0:1: [sda] Attached SCSI removable disk
[   12.460754] EXT4-fs (mmcblk0p2): recovery complete
[   12.473571] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[   12.482086] VFS: Mounted root (ext4 filesystem) on device 179:2.
[   12.489440] Freeing init memory: 620K
[   12.518524] init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
[   12.623168] init: cannot open '/initlogo.rle'
[   12.711608] Disabling lock debugging due to kernel taint
[   12.717895] Compat-wireless backport release: ol_R5.00.21
[   12.723571] Backport based on wl12xx.git ol_R5.00.21
[   12.764160] cfg80211: Calling CRDA to update world regulatory domain
[   12.879119] wl12xx: driver version:
[   12.882934] wl12xx: compilation time: Thu Mar 21 22:43:49 2013
[   12.916046] init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
[   12.926239] android_usb: already disabled
[   12.930694] adb_bind_config
[   13.808410] cfg80211: World regulatory domain updated:
[   13.813873] cfg80211:     (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
[   13.822601] cfg80211:     (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
[   13.830871] cfg80211:     (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
[   13.839141] cfg80211:     (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
[   13.847412] cfg80211:     (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
[   13.855682] cfg80211:     (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
[   14.749145] adb_open
root@android:/ # [   15.540588] init: untracked pid 71 exited
[  167.720855] warning: `zygote' uses 32-bit capabilities (legacy support in use)
[  363.324005] request_suspend_state: wakeup (3->0) at 363320941580 (2000-01-01 00:06:01.784932814 UTC)
[  404.021484] acc_open
[  404.024047] acc_release
[  431.747680] alarm_release: clear alarm, pending 0
[  431.752716] binder: release 167:167 transaction 37373 in, still active
[  431.759613] binder: send failed reply for transaction 37373 to 313:313
[  431.772644] binder: 313:313 transaction failed 29189, size 64-0
[  431.791076] request_suspend_state: wakeup (0->0) at 431788013114 (2000-01-01 00:07:10.252004348 UTC)
[  431.815002] init: untracked pid 67 exited
[  431.823822] init: untracked pid 73 exited
[  431.828796] init: untracked pid 313 exited
[  441.380126] request_suspend_state: wakeup (0->0) at 441377063406 (2000-01-01 00:07:19.841054641 UTC)
[  441.401000] init: untracked pid 334 exited
[  441.410552] init: untracked pid 335 exited
[  442.608032] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[  442.614929] PVR_K: SGX debug (blaze_android_sgx_ogles1_ogles2_GPL sgxddk 18 1.8@789263)
[  442.623291] PVR_K: (P0) EUR_CR_CORE_ID:          01120000
[  442.628936] PVR_K: (P0) EUR_CR_CORE_REVISION:    00010205
[  442.634582] PVR_K: (P0) EUR_CR_EVENT_STATUS:     20000000
[  442.640228] PVR_K: (P0) EUR_CR_EVENT_STATUS2:    00000008
[  442.645874] PVR_K: (P0) EUR_CR_BIF_CTRL:         00000000
[  442.651519] PVR_K: (P0) EUR_CR_BIF_INT_STAT:     00000000
[  442.657165] PVR_K: (P0) EUR_CR_BIF_FAULT:        00000000
[  442.662780] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[  442.668457] PVR_K: (P0) EUR_CR_CLKGATECTL:       00222220
[  442.674102] PVR_K: (P0) EUR_CR_PDS_PC_BASE:      0030000C
[  442.679748] PVR_K: Flip Command Complete Data 0 for display device 1:
[  442.686492] PVR_K:   SRC 0: (Not in use)
[  442.690490] PVR_K:   SRC 1: (Not in use)
[  442.694519] PVR_K: Flip Command Complete Data 1 for display device 1:
[  442.701232] PVR_K:   SRC 0: (Not in use)
[  442.705261] PVR_K:   SRC 1: (Not in use)
[  442.709259] PVR_K: SGX Host control:
[  442.712982] PVR_K:   (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[  442.719818] PVR_K:   (HC-10) 0x00000001 0x00000000 0x0000000A 0x00030D40
[  442.726745] PVR_K:   (HC-20) 0x00000065 0x00000001 0x00000001 0x00000000
[  442.733673] PVR_K:   (HC-30) 0x00000002 0x0006467D 0xEFFFA020 0x00000000
[  442.740570] PVR_K:   (HC-40) 0x00000000 0x00000000 0xFBEBFFFF 0xFFFF67FD
[  442.747497] PVR_K: SGX TA/3D control:
[  442.751312] PVR_K:   (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[  442.758239] PVR_K:   (T3C-10) 0x00000000 0x00000001 0x00000002 0x00000001
[  442.765258] PVR_K:   (T3C-20) 0x0F0AD4E0 0x00000000 0x00000000 0x00000000
[  442.772247] PVR_K:   (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[  442.779266] PVR_K:   (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[  442.786285] PVR_K:   (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[  442.793273] PVR_K:   (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[  442.800292] PVR_K:   (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[  442.807312] PVR_K:   (T3C-80) 0x00000000 0x0F0D0538 0x00000000 0x0F000000
[  442.814300] PVR_K:   (T3C-90) 0x8F32F000 0x0F0BE400 0x00000000 0x0F08BB40
[  442.821319] PVR_K:   (T3C-A0) 0x0F0AD4E0 0x0F0D0538 0x0F08BB40 0x00000000
[  442.828338] PVR_K:   (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[  442.835327] PVR_K:   (T3C-C0) 0x00000000 0x00000000 0x00000000 0x0000133F
[  442.842346] PVR_K:   (T3C-D0) 0x0000133F 0x0F000000 0x8000B000 0x8004B000
[  442.849365] PVR_K:   (T3C-E0) 0x0F004000 0x0F00A420 0x0F00A740 0x0F08B6C0
[  442.856353] PVR_K:   (T3C-F0) 0x0F08B6C0 0x00000000 0x0000007E 0x0000007E
[  442.863372] PVR_K:   (T3C-100) 0x00000000 0x00000001 0x00000000 0x00000000
[  442.870483] PVR_K:   (T3C-110) 0x00000000 0x52DA6D94 0xF7FFFFBF 0xFDFFFBFF
[  442.877563] PVR_K: SGX Kernel CCB WO:0xC3 RO:0xC3
[  444.240661] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[  444.247558] PVR_K: SGX debug (blaze_android_sgx_ogles1_ogles2_GPL sgxddk 18 1.8@789263)
[  444.255920] PVR_K: (P0) EUR_CR_CORE_ID:          01120000
[  444.261566] PVR_K: (P0) EUR_CR_CORE_REVISION:    00010205
[  444.267211] PVR_K: (P0) EUR_CR_EVENT_STATUS:     20000000
[  444.272857] PVR_K: (P0) EUR_CR_EVENT_STATUS2:    00000008
[  444.278503] PVR_K: (P0) EUR_CR_BIF_CTRL:         00000000
[  444.284149] PVR_K: (P0) EUR_CR_BIF_INT_STAT:     00000000
[  444.289794] PVR_K: (P0) EUR_CR_BIF_FAULT:        00000000
[  444.295440] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[  444.301086] PVR_K: (P0) EUR_CR_CLKGATECTL:       00222220
[  444.306732] PVR_K: (P0) EUR_CR_PDS_PC_BASE:      002033A4
[  444.312377] PVR_K: Flip Command Complete Data 0 for display device 1:
[  444.319091] PVR_K:   SRC 0: (Not in use)
[  444.323120] PVR_K:   SRC 1: (Not in use)
[  444.327117] PVR_K: Flip Command Complete Data 1 for display device 1:
[  444.333862] PVR_K:   SRC 0: (Not in use)
[  444.337860] PVR_K:   SRC 1: (Not in use)
[  444.341857] PVR_K: SGX Host control:
[  444.345611] PVR_K:   (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[  444.352416] PVR_K:   (HC-10) 0x00000002 0x00000000 0x0000000A 0x00030D40
[  444.359344] PVR_K:   (HC-20) 0x00000065 0x00000001 0x00000001 0x00000000
[  444.366241] PVR_K:   (HC-30) 0x00000002 0x00064BCB 0x088405F0 0x00000000
[  444.373168] PVR_K:   (HC-40) 0x00000000 0x00000000 0xFBEBFFFF 0xFFFF67FD
[  444.380065] PVR_K: SGX TA/3D control:
[  444.383911] PVR_K:   (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[  444.390808] PVR_K:   (T3C-10) 0x00000000 0x00000001 0x00000002 0x00000001
[  444.397827] PVR_K:   (T3C-20) 0x0F0AD4E0 0x00000000 0x00000000 0x00000000
[  444.404815] PVR_K:   (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[  444.411834] PVR_K:   (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[  444.418823] PVR_K:   (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[  444.425842] PVR_K:   (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[  444.432830] PVR_K:   (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[  444.439819] PVR_K:   (T3C-80) 0x00000000 0x0F0D0578 0x00000000 0x0F000000
[  444.446838] PVR_K:   (T3C-90) 0x8F32F000 0x0F0BB000 0x00000000 0x0F08BB40
[  444.453857] PVR_K:   (T3C-A0) 0x0F0AD4E0 0x0F0D0578 0x0F08BB40 0x00000000
[  444.460845] PVR_K:   (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[  444.467834] PVR_K:   (T3C-C0) 0x00000000 0x00000000 0x00000000 0x00001350
[  444.474853] PVR_K:   (T3C-D0) 0x00001350 0x0F000000 0x8000B000 0x8004B000
[  444.481842] PVR_K:   (T3C-E0) 0x0F004000 0x0F00A420 0x0F00A740 0x0F08B6C0
[  444.488861] PVR_K:   (T3C-F0) 0x0F08B6C0 0x00000000 0x0000007E 0x0000007E
[  444.495880] PVR_K:   (T3C-100) 0x00000000 0x00000001 0x00000000 0x00000000
[  444.502960] PVR_K:   (T3C-110) 0x00000000 0x23DA7C52 0xF7FFFFBF 0xFDFFFBFF
[  444.510040] PVR_K: SGX Kernel CCB WO:0x3B RO:0x3B
[  497.202270] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[  497.209136] PVR_K: SGX debug (blaze_android_sgx_ogles1_ogles2_GPL sgxddk 18 1.8@789263)
[  497.217529] PVR_K: (P0) EUR_CR_CORE_ID:          01120000
[  497.223175] PVR_K: (P0) EUR_CR_CORE_REVISION:    00010205
[  497.228820] PVR_K: (P0) EUR_CR_EVENT_STATUS:     20000000
[  497.234466] PVR_K: (P0) EUR_CR_EVENT_STATUS2:    00000008
[  497.240081] PVR_K: (P0) EUR_CR_BIF_CTRL:         00000000
[  497.245727] PVR_K: (P0) EUR_CR_BIF_INT_STAT:     00000000
[  497.251373] PVR_K: (P0) EUR_CR_BIF_FAULT:        00000000
[  497.257019] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[  497.262634] PVR_K: (P0) EUR_CR_CLKGATECTL:       00222220
[  497.268280] PVR_K: (P0) EUR_CR_PDS_PC_BASE:      00000000
[  497.273925] PVR_K: Flip Command Complete Data 0 for display device 1:
[  497.280670] PVR_K:   SRC 0: (Not in use)
[  497.284667] PVR_K:   SRC 1: (Not in use)
[  497.288665] PVR_K: Flip Command Complete Data 1 for display device 1:
[  497.295410] PVR_K:   SRC 0: (Not in use)
[  497.299407] PVR_K:   SRC 1: (Not in use)
[  497.303405] PVR_K: SGX Host control:
[  497.307159] PVR_K:   (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[  497.313964] PVR_K:   (HC-10) 0x00000003 0x00000000 0x0000000A 0x00030D40
[  497.320861] PVR_K:   (HC-20) 0x00000065 0x00000001 0x00000001 0x00000000
[  497.327789] PVR_K:   (HC-30) 0x00000002 0x0007199A 0x089D0C30 0x00000000
[  497.334716] PVR_K:   (HC-40) 0x00000000 0x00000000 0xFBEBFFFF 0xFFFF67FD
[  497.341613] PVR_K: SGX TA/3D control:
[  497.345428] PVR_K:   (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[  497.352355] PVR_K:   (T3C-10) 0x00000000 0x00000001 0x00000002 0x00000001
[  497.359344] PVR_K:   (T3C-20) 0x0F0AD4E0 0x00000000 0x00000000 0x00000000
[  497.366363] PVR_K:   (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[  497.373352] PVR_K:   (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[  497.380340] PVR_K:   (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[  497.387359] PVR_K:   (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[  497.394348] PVR_K:   (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[  497.401367] PVR_K:   (T3C-80) 0x00000000 0x0F0D0578 0x00000000 0x0F000000
[  497.408355] PVR_K:   (T3C-90) 0x8F32F000 0x0F0B5000 0x00000000 0x0F08BB40
[  497.415374] PVR_K:   (T3C-A0) 0x0F0AD4E0 0x0F0D0578 0x0F08BB40 0x00000000
[  497.422363] PVR_K:   (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[  497.429351] PVR_K:   (T3C-C0) 0x00000000 0x00000000 0x00000000 0x000015C8
[  497.436370] PVR_K:   (T3C-D0) 0x000015C8 0x0F000000 0x8000B000 0x8004B000
[  497.443359] PVR_K:   (T3C-E0) 0x0F004000 0x0F00A420 0x0F00A740 0x0F08B6C0
[  497.450347] PVR_K:   (T3C-F0) 0x0F08B6C0 0x00000000 0x0000007E 0x0000007E
[  497.457366] PVR_K:   (T3C-100) 0x00000000 0x00000001 0x00000001 0x00000000
[  497.464477] PVR_K:   (T3C-110) 0x00000000 0xF1656BAD 0xF7FFFFBF 0xFDFFFBFF
[  497.471557] PVR_K: SGX Kernel CCB WO:0x84 RO:0x84
[  499.580566] request_suspend_state: wakeup (0->0) at 499577502858 (2000-01-01 00:08:18.041524610 UTC)
[  515.132110] acc_open
[  515.134613] acc_release
[  521.626739] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[  521.633636] PVR_K: SGX debug (blaze_android_sgx_ogles1_ogles2_GPL sgxddk 18 1.8@789263)
[  521.641998] PVR_K: (P0) EUR_CR_CORE_ID:          01120000
[  521.647644] PVR_K: (P0) EUR_CR_CORE_REVISION:    00010205
[  521.653289] PVR_K: (P0) EUR_CR_EVENT_STATUS:     20000000
[  521.658935] PVR_K: (P0) EUR_CR_EVENT_STATUS2:    00000008
[  521.664581] PVR_K: (P0) EUR_CR_BIF_CTRL:         00000000
[  521.670196] PVR_K: (P0) EUR_CR_BIF_INT_STAT:     00000000
[  521.675842] PVR_K: (P0) EUR_CR_BIF_FAULT:        00000000
[  521.681488] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[  521.687133] PVR_K: (P0) EUR_CR_CLKGATECTL:       00222220
[  521.692779] PVR_K: (P0) EUR_CR_PDS_PC_BASE:      002033A4
[  521.698425] PVR_K: Flip Command Complete Data 0 for display device 1:
[  521.705139] PVR_K:   SRC 0: (Not in use)
[  521.709167] PVR_K:   SRC 1: (Not in use)
[  521.713165] PVR_K: Flip Command Complete Data 1 for display device 1:
[  521.719879] PVR_K:   SRC 0: (Not in use)
[  521.723907] PVR_K:   SRC 1: (Not in use)
[  521.727905] PVR_K: SGX Host control:
[  521.731628] PVR_K:   (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[  521.738464] PVR_K:   (HC-10) 0x00000004 0x00000000 0x0000000A 0x00030D40
[  521.745361] PVR_K:   (HC-20) 0x00000065 0x00000001 0x00000001 0x00000000
[  521.752288] PVR_K:   (HC-30) 0x00000002 0x000777F0 0x0BC52730 0x00000000
[  521.759185] PVR_K:   (HC-40) 0x00000000 0x00000000 0xFBEBFFFF 0xFFFF67FD
[  521.766113] PVR_K: SGX TA/3D control:
[  521.769927] PVR_K:   (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[  521.776855] PVR_K:   (T3C-10) 0x00000000 0x00000001 0x00000002 0x00000001
[  521.783843] PVR_K:   (T3C-20) 0x0F0AD4E0 0x00000000 0x00000000 0x00000000
[  521.790832] PVR_K:   (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[  521.797851] PVR_K:   (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[  521.804840] PVR_K:   (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[  521.811828] PVR_K:   (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[  521.818847] PVR_K:   (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[  521.825836] PVR_K:   (T3C-80) 0x00000000 0x0F0D0578 0x00000000 0x0F000000
[  521.832855] PVR_K:   (T3C-90) 0x8F32F000 0x0F0BE800 0x00000000 0x0F08BB40
[  521.839843] PVR_K:   (T3C-A0) 0x0F0AD4E0 0x0F0D0578 0x0F08BB40 0x00000000
[  521.846862] PVR_K:   (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[  521.853851] PVR_K:   (T3C-C0) 0x00000000 0x00000000 0x00000000 0x000016EA
[  521.860870] PVR_K:   (T3C-D0) 0x000016EA 0x0F000000 0x8000B000 0x8004B000
[  521.867858] PVR_K:   (T3C-E0) 0x0F004000 0x0F00A420 0x0F00A740 0x0F08B6C0
[  521.874877] PVR_K:   (T3C-F0) 0x0F08B6C0 0x00000000 0x0000007E 0x0000007E
[  521.881866] PVR_K:   (T3C-100) 0x00000000 0x00000001 0x00000000 0x00000000
[  521.888946] PVR_K:   (T3C-110) 0x00000000 0x08F89F60 0xF7FFFFBF 0xFDFFFBFF
[  521.896087] PVR_K: SGX Kernel CCB WO:0x73 RO:0x73
[  535.438201] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[  535.445068] PVR_K: SGX debug (blaze_android_sgx_ogles1_ogles2_GPL sgxddk 18 1.8@789263)
[  535.453460] PVR_K: (P0) EUR_CR_CORE_ID:          01120000
[  535.459075] PVR_K: (P0) EUR_CR_CORE_REVISION:    00010205
[  535.464721] PVR_K: (P0) EUR_CR_EVENT_STATUS:     20000000
[  535.470367] PVR_K: (P0) EUR_CR_EVENT_STATUS2:    00000008
[  535.476013] PVR_K: (P0) EUR_CR_BIF_CTRL:         00000000
[  535.481628] PVR_K: (P0) EUR_CR_BIF_INT_STAT:     00000000
[  535.487274] PVR_K: (P0) EUR_CR_BIF_FAULT:        00000000
[  535.492919] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[  535.498565] PVR_K: (P0) EUR_CR_CLKGATECTL:       00222220
[  535.504211] PVR_K: (P0) EUR_CR_PDS_PC_BASE:      002033A4
[  535.509857] PVR_K: Flip Command Complete Data 0 for display device 1:
[  535.516571] PVR_K:   SRC 0: (Not in use)
[  535.520599] PVR_K:   SRC 1: (Not in use)
[  535.524597] PVR_K: Flip Command Complete Data 1 for display device 1:
[  535.531311] PVR_K:   SRC 0: (Not in use)
[  535.535339] PVR_K:   SRC 1: (Not in use)
[  535.539337] PVR_K: SGX Host control:
[  535.543090] PVR_K:   (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[  535.549896] PVR_K:   (HC-10) 0x00000005 0x00000000 0x0000000A 0x00030D40
[  535.556823] PVR_K:   (HC-20) 0x00000065 0x00000001 0x00000001 0x00000000
[  535.563720] PVR_K:   (HC-30) 0x00000002 0x0007ACD1 0x0D39C5D0 0x00000000
[  535.570617] PVR_K:   (HC-40) 0x00000000 0x00000000 0xFBEBFFFF 0xFFFF67FD
[  535.577545] PVR_K: SGX TA/3D control:
[  535.581359] PVR_K:   (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[  535.588287] PVR_K:   (T3C-10) 0x00000000 0x00000001 0x00000002 0x00000001
[  535.595275] PVR_K:   (T3C-20) 0x0F0AD4E0 0x00000000 0x00000000 0x00000000
[  535.602294] PVR_K:   (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[  535.609283] PVR_K:   (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[  535.616302] PVR_K:   (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[  535.623291] PVR_K:   (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[  535.630279] PVR_K:   (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[  535.637298] PVR_K:   (T3C-80) 0x00000000 0x0F0D0538 0x00000000 0x0F000000
[  535.644317] PVR_K:   (T3C-90) 0x8F32F000 0x0F0B8C00 0x00000000 0x0F08BB40
[  535.651306] PVR_K:   (T3C-A0) 0x0F0AD4E0 0x0F0D0538 0x0F08BB40 0x00000000
[  535.658325] PVR_K:   (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[  535.665313] PVR_K:   (T3C-C0) 0x00000000 0x00000000 0x00000000 0x0000178D
[  535.672302] PVR_K:   (T3C-D0) 0x0000178D 0x0F000000 0x8000B000 0x8004B000
[  535.679321] PVR_K:   (T3C-E0) 0x0F004000 0x0F00A420 0x0F00A740 0x0F08B6C0
[  535.686309] PVR_K:   (T3C-F0) 0x0F08B6C0 0x00000000 0x0000007E 0x0000007E
[  535.693328] PVR_K:   (T3C-100) 0x00000000 0x00000001 0x00000000 0x00000000
[  535.700408] PVR_K:   (T3C-110) 0x00000000 0x5DE1896B 0xF7FFFFBF 0xFDFFFBFF
[  535.707519] PVR_K: SGX Kernel CCB WO:0xE9 RO:0xE9
[  634.539916] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[  634.546813] PVR_K: SGX debug (blaze_android_sgx_ogles1_ogles2_GPL sgxddk 18 1.8@789263)
[  634.555175] PVR_K: (P0) EUR_CR_CORE_ID:          01120000
[  634.560821] PVR_K: (P0) EUR_CR_CORE_REVISION:    00010205
[  634.566467] PVR_K: (P0) EUR_CR_EVENT_STATUS:     20000000
[  634.572113] PVR_K: (P0) EUR_CR_EVENT_STATUS2:    00000008
[  634.577758] PVR_K: (P0) EUR_CR_BIF_CTRL:         00000000
[  634.583404] PVR_K: (P0) EUR_CR_BIF_INT_STAT:     00000000
[  634.589050] PVR_K: (P0) EUR_CR_BIF_FAULT:        00000000
[  634.594696] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[  634.600341] PVR_K: (P0) EUR_CR_CLKGATECTL:       00222220
[  634.605987] PVR_K: (P0) EUR_CR_PDS_PC_BASE:      00000000
[  634.611633] PVR_K: Flip Command Complete Data 0 for display device 1:
[  634.618347] PVR_K:   SRC 0: (Not in use)
[  634.622375] PVR_K:   SRC 1: (Not in use)
[  634.626373] PVR_K: Flip Command Complete Data 1 for display device 1:
[  634.633117] PVR_K:   SRC 0: (Not in use)
[  634.637115] PVR_K:   SRC 1: (Not in use)
[  634.641113] PVR_K: SGX Host control:
[  634.644866] PVR_K:   (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[  634.651672] PVR_K:   (HC-10) 0x00000006 0x00000000 0x0000000A 0x00030D40
[  634.658599] PVR_K:   (HC-20) 0x00000065 0x00000001 0x00000001 0x00000000
[  634.665496] PVR_K:   (HC-30) 0x00000002 0x00092EDC 0x0E0C7F20 0x00000000
[  634.672424] PVR_K:   (HC-40) 0x00000000 0x00000000 0xFBEBFFFF 0xFFFF67FD
[  634.679321] PVR_K: SGX TA/3D control:
[  634.683166] PVR_K:   (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[  634.690063] PVR_K:   (T3C-10) 0x00000000 0x00000001 0x00000002 0x00000001
[  634.697052] PVR_K:   (T3C-20) 0x0F0AD4E0 0x00000000 0x00000000 0x00000000
[  634.704071] PVR_K:   (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[  634.711059] PVR_K:   (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[  634.718078] PVR_K:   (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[  634.725067] PVR_K:   (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[  634.732086] PVR_K:   (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[  634.739074] PVR_K:   (T3C-80) 0x00000000 0x0F0D0578 0x00000000 0x0F000000
[  634.746093] PVR_K:   (T3C-90) 0x8F32F000 0x0F0B1800 0x00000000 0x0F08BB40
[  634.753082] PVR_K:   (T3C-A0) 0x0F0AD4E0 0x0F0D0578 0x0F08BB40 0x00000000
[  634.760101] PVR_K:   (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[  634.767089] PVR_K:   (T3C-C0) 0x00000000 0x00000000 0x00000000 0x00001C2E
[  634.774108] PVR_K:   (T3C-D0) 0x00001C2E 0x0F000000 0x8000B000 0x8004B000
[  634.781097] PVR_K:   (T3C-E0) 0x0F004000 0x0F00A420 0x0F00A740 0x0F08B6C0
[  634.788116] PVR_K:   (T3C-F0) 0x0F08B6C0 0x00000000 0x0000007E 0x0000007E
[  634.795104] PVR_K:   (T3C-100) 0x00000000 0x00000001 0x00000000 0x00000000
[  634.802185] PVR_K:   (T3C-110) 0x00000000 0xDBA58FD6 0xF7FFFFBF 0xFDFFFBFF
[  634.809295] PVR_K: SGX Kernel CCB WO:0x58 RO:0x58
[  652.207427] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[  652.214324] PVR_K: SGX debug (blaze_android_sgx_ogles1_ogles2_GPL sgxddk 18 1.8@789263)
[  652.222656] PVR_K: (P0) EUR_CR_CORE_ID:          01120000
[  652.228332] PVR_K: (P0) EUR_CR_CORE_REVISION:    00010205
[  652.233947] PVR_K: (P0) EUR_CR_EVENT_STATUS:     20000000
[  652.239593] PVR_K: (P0) EUR_CR_EVENT_STATUS2:    00000008
[  652.245239] PVR_K: (P0) EUR_CR_BIF_CTRL:         00000000
[  652.250854] PVR_K: (P0) EUR_CR_BIF_INT_STAT:     00000000
[  652.256500] PVR_K: (P0) EUR_CR_BIF_FAULT:        00000000
[  652.262145] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[  652.267791] PVR_K: (P0) EUR_CR_CLKGATECTL:       00222220
[  652.273437] PVR_K: (P0) EUR_CR_PDS_PC_BASE:      002033A4
[  652.279083] PVR_K: Flip Command Complete Data 0 for display device 1:
[  652.285797] PVR_K:   SRC 0: (Not in use)
[  652.289794] PVR_K:   SRC 1: (Not in use)
[  652.293823] PVR_K: Flip Command Complete Data 1 for display device 1:
[  652.300537] PVR_K:   SRC 0: (Not in use)
[  652.304565] PVR_K:   SRC 1: (Not in use)
[  652.308593] PVR_K: SGX Host control:
[  652.312316] PVR_K:   (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[  652.319122] PVR_K:   (HC-10) 0x00000007 0x00000000 0x0000000A 0x00030D40
[  652.326049] PVR_K:   (HC-20) 0x00000065 0x00000001 0x00000001 0x00000000
[  652.332946] PVR_K:   (HC-30) 0x00000002 0x000972CD 0x13F4CB90 0x00000000
[  652.339874] PVR_K:   (HC-40) 0x00000000 0x00000000 0xFBEBFFFF 0xFFFF67FD
[  652.346771] PVR_K: SGX TA/3D control:
[  652.350616] PVR_K:   (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[  652.357513] PVR_K:   (T3C-10) 0x00000000 0x00000001 0x00000002 0x00000001
[  652.364532] PVR_K:   (T3C-20) 0x0F0AD4E0 0x00000000 0x00000000 0x00000000
[  652.371520] PVR_K:   (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[  652.378509] PVR_K:   (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[  652.385528] PVR_K:   (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[  652.392517] PVR_K:   (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[  652.399505] PVR_K:   (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[  652.406524] PVR_K:   (T3C-80) 0x00000000 0x0F0D0538 0x00000000 0x0F000000
[  652.413543] PVR_K:   (T3C-90) 0x8F32F000 0x0F0BE400 0x00000000 0x0F08BB40
[  652.420532] PVR_K:   (T3C-A0) 0x0F0AD4E0 0x0F0D0538 0x0F08BB40 0x00000000
[  652.427520] PVR_K:   (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[  652.434539] PVR_K:   (T3C-C0) 0x00000000 0x00000000 0x00000000 0x00001CFF
[  652.441528] PVR_K:   (T3C-D0) 0x00001CFF 0x0F000000 0x8000B000 0x8004B000
[  652.448547] PVR_K:   (T3C-E0) 0x0F004000 0x0F00A420 0x0F00A740 0x0F08B6C0
[  652.455535] PVR_K:   (T3C-F0) 0x0F08B6C0 0x00000000 0x0000007E 0x0000007E
[  652.462524] PVR_K:   (T3C-100) 0x00000000 0x00000001 0x00000000 0x00000000
[  652.469635] PVR_K:   (T3C-110) 0x00000000 0xA773C3B9 0xF7FFFFBF 0xFDFFFBFF
[  652.476715] PVR_K: SGX Kernel CCB WO:0x10 RO:0x10
[  701.128356] binder: 627: binder_alloc_buf, no vma
[  701.133361] binder: 388:625 transaction failed 29201, size 4-0
[  701.139465] binder: send failed reply for transaction 61581 to 627:627
[  701.150909] binder: 620: binder_alloc_buf, no vma
[  701.155944] binder: 388:623 transaction failed 29201, size 4-0
[  701.162048] binder: send failed reply for transaction 61446 to 620:620
[  702.659942] binder: release 589:589 transaction 65882 out, still active
[  820.342987] binder: release 794:854 transaction 71569 out, still active
[  847.133453] binder: 388:653 transaction failed 29189, size 1084-4
[  847.139862] binder: send failed reply for transaction 71569, target dead
root@android:/ # [  986.887878] binder: 120:120 transaction failed 29189, size 164-0