This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Series Capacitors on Hyperlink Interface

Hi,

Do I have to place series capacitors on the Hyperlink SerDes if the two C6678 device's power supply comes from the same source?

Thanks,

Noam

  • In the configuration you described the series capacitor is not required.  This is only true for the Hyperlink SerDes interface and only when connecting one KeyStone I device to another.

  • Hi Bill

    I see you have very kindly answered a question regarding series capacitors on Hyperlink interfaces - I too have asked a question regarding the physical placement of capacitors on a Hyperlink interface, particularly between two boards connected by a high speed connector. I wondered if you had seen this question and if you have any useful comments for us as we are now in PCB layout.

    http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/439/t/253523.aspx

    I hope to hear from you,

    Kind regards

    Chris S.