This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6474 EMAC PHY



Dear Sir:

I have made C6457 EMAC with Vitesse VSC8221 PHY working by using ti_ndk_src_2_1_0 and ti.ndk.platforms.evm6457_2_0_0. Then I tried to use the same PHY device with C6474 EMAC. The software packages used are ti_ndk_src_2_1_0 and ti.ndk.platforms.evm6474_2_1_0.

Unfortunately, I couldn't ping the IP address even the Link status is OK as following:

TCP/IP Stack Example Client
MAC Address read from EFUSE: 00-24-ba-0d-43-3c
Core Number on which NDK is running = 0
EFUSED MAC Address = 00-24-ba-0d-43-3c
Only on CORE 0: SGMII reset successful........
Only on CORE 0: SGMII config successful........
Only on CORE 0: SerDes should be up and running
EMAC has been started successfully
Registeration of the EMAC Successful
Network Added: If-1:192.168.1.42
Service Status: Telnet : Enabled : : 000
Service Status: HTTP : Enabled : : 000
Link Status: 100Mb/s Full Duplex on PHY 0

Anyone could help to point out a way for me?

Thanks in advance.