Hi,
I am using RDK2.8.
In the swosd example, when blend the window, the DMA move the data from the address of pInA which is the offset address of the videoWindowAddr and the address of pInB which is the graphicsWindowAddr to the out address pInA.
Now I confused about which address I should set the DMA move to?
Are there any examples about how to use the DMA to move the data to L2 memory and then process them? Can the example SCD or audio demo be helpful?
Sincerely Thanks !
Best Regards !