This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 not found image



Dear all

My system is DM368 IPNC Ver4.0.

When i boot with UBIFS file system, some boards are OK but some boards are making kernel panic.

Below is my log.

U-Boot 1.3.4 (Jun 9 2012 - 17:24:47) DM368-IPNC-4.0.0

I2C: ready
DRAM: 128 MB
NAND: NAND device: Manufacturer ID: 0xec, Chip ID: 0xf1 (Samsung NAND 128MiB 3,3V 8-bit)
Bad block table not found for chip 0
Bad block table not found for chip 0

loop oob 81021ad8 Bad block table written to 0x07fe0000, version 0x01

loop oob 81021ad8 Bad block table written to 0x07fc0000, version 0x01
128 MiB
In: serial
Out: serial
Err: serial
ARM Clock :- 432MHz
DDR Clock :- 340MHz
Ethernet PHY: GENERIC @ 0x01
Hit any key to stop autoboot: 0

Loading from NAND 128MiB 3,3V 8-bit, offset 0x500000
Image Name: Linux-2.6.37_IPNC_DM365_4.0.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3439968 Bytes = 3.3 MB
Load Address: 80008000
Entry Point: 80008000
## Booting kernel from Legacy Image at 80700000 ...
Image Name: Linux-2.6.37_IPNC_DM365_4.0.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3439968 Bytes = 3.3 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK

Starting kernel ...

[ 0.000000] UBI error: incorrect bytes count: ""
[ 0.000000] Booting kernel: `3,' invalid for parameter `ubi.mtd'
[ 0.746489] Error: Driver 'davinci-mcbsp' is already registered, aborting...
[ 87.649976] IP-Config: Reopening network devices...
[ 174.729968] IP-Config: Auto-configuration of network failed.
[ 174.736857] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
[ 174.745227] Backtrace: 
[ 174.747704] Function entered at [<c002c4ec>] from [<c02bf974>]
[ 174.753630] r7:00008000 r6:c4013000 r5:c002295c r4:c03504c0
[ 174.759411] Function entered at [<c02bf95c>] from [<c02bf9e0>]
[ 174.765252] Function entered at [<c02bf978>] from [<c0008f8c>]
[ 174.771151] r3:00000000 r2:00000000 r1:c4027f60 r0:c02dc1b9
[ 174.776854] Function entered at [<c0008d20>] from [<c000903c>]
[ 174.782753] Function entered at [<c0008fe8>] from [<c00091b4>]
[ 174.788596] r5:c00220f8 r4:c034fdc8
[ 174.792257] Function entered at [<c0009054>] from [<c00084b4>]
[ 174.798094] r5:c00220f8 r4:c034fd78
[ 174.801752] Function entered at [<c00083a4>] from [<c0040e0c>]
[ 174.807590] r5:c00083a4 r4:00000000

Thanks in advance.

Hennessy