Hi,
I do PSNR testing with TI's h264 HP encoder in two enropy coding type using the encoding
configuration(3Mbps, 4 slice fps=30 no intra_refresh, test sequence:mobcal http://media.xiph.org/video/derf/).
The test result is below: CABAC: PSNR = 35.323db, CAVLC = 34.653. So there is about 0.67db
improvement with CABAC versus CAVLC. I do the same testing on x.264 encoder and find the difference
is only 0.2db. So I wonder what is the reason causing the improvement.
Thanks!
B.R.
Sunzhao