This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM648 DDR2 Clock (PLL2) Issue

In the our customer boards, the PLL2 Controller Input Clock (CLKIN2) frequency is 26.6MHz.
In this case the DDR2 Memory Controller Output Clock frequency (DDR_CLKP/N) must be 266MHz.
However it often showed 13.3MHz.
When the AEA19 pin is externally pulled up this issue is not shown.

In the DM648 EVM, the AEA19 pin is PLLBYPASS2 Boot mode signal (SW3-1).
It is related to PLL2 bypass mode (DDR2 clock).
When it shows Low, the DDR_CLKP/N frequency show 13.3MHz.
Note when SW3-1 is set to OFF it does not show Low because the external pull down is weak.

Must the AEA19 pin be externally pulled up?

Best regards,

Daisuke