This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5515 ezDSP integrating SD save with audio



I have been working with the C5515 ezDSP trying to implement a simple audio recorder.  I can get all of the example SD record functions to work, as well as the Audio Filter demo which works.  When I try to integrate the CSL MMCSD DMA example into this code, I run into some trouble.
First, I believe the Audio Filter demo may be using different versions of DMA than the CSL DMA calls.  Is this correct?

Second, if I call just MMC_init();, the audio data stops streaming, but the code is otherwise running (LED normally turns on and off every 10 seconds).

Does anyone have a working version of a simple audio recorder for this board?  It seems like something TI should offer to get people up running quickly.  This forum seems to have a lot of people that have the same problem.  My hope is that someone has cracked this nut and is willing to post their code.