Hey,
I have a design using AM3359ZCZ and the problem is that I found 2 boards (out of twelve I have made) have the following same booting issue:
After pressing the reset bottom, the console( via serial port) immediately shows "U-Boot SPL 2012.10-00010-g847bb01 (Oct 25 2012 -11:41:49)"
and then it hangs, but after a while it continues to boot normally, the period is uncertain and can range from several seconds to several minutes.
I guess it maybe a soldering issue, does anyone have the same problem before, thanks!
PS:
The design is based on beagle bone, it has 256M ram and boots from uSD card.
Thanks!
Qi