Other Parts Discussed in Thread: TM4C123GH6PGE, SYSBIOS
Hi,
I am currently using a LM3S9D92 part with the TI-RTOS 1.1.0.25 package. I am trying to implement a system, using FatFS, to read and write files to/from a USB flash drive (mass storage device). I am able to mount the drive, read, write, seek -- all the standard I/O functions. However, with certain USB drives, I seem to be creating a sort of "hidden" partition.
What I mean by a hidden partition is that Windows seems to ignore it. When the USB drive is plugged into my board with the 9D92, I am able to interact with the drive as I would normally expect. I am able to read and create directories, read from existing files, create new files, etc. However, when I plug the drive into a Windows machine, it shows up as an empty drive. No folders, no files -- nothing. It allows me to create folders and files on the drive with Windows, but when I plug the drive back into my 9D92 board, the files are nowhere to be found -- the only files I can see are the ones I created with my board.
So, what I seem to have is what I would call two partitions -- one being used by my 9D92 board, and one being used by Windows. I would venture to guess that it has something to do with how I'm mounting and initializing the USB drive, but I followed example DK_LM3S9D96_fatsdusbcopy for all of my initialization, so I have no idea what I'm doing wrong.
Has anyone run into this issue before? Any insight would be greatly appreciated.
Thanks,
Mitch