when I use AAC-LC encoder to encode one 48KHz stereo audio(128Kbps), I found the DSP CPU Load up to 99%,
the efficiency is poor.where is wrong?
I am using DVR RDK 3.50.00.05.
*************Capture Buf Size 8192, Enc Buffer Size 2048
AUDIO: ENC Handle 8EA00, Int Handle 8EA0C
AUDIO: ENC -> bitrate 131072 inputBitsPerSample 16, sampleRate - 48000, numberOfChannels - 2...
AUDIO: ENC -> Rpe_create(AAC_ENC) done....
AUDIO: CAPTURE -> Encoder creation SUCCESS for CH - 0
AUDIO: Audio_startCapture() success....
[c6xdsp ]
[c6xdsp ] 103447: LOAD: CPU: 99.2% HWI: 3.2%, SWI:3.1%
[c6xdsp ]
[c6xdsp ] 103910: LOAD: TSK: SYSTEM : 0.3%
[c6xdsp ] 104365: LOAD: TSK: MISC : 92.6%
[c6xdsp ]
Thanks.
CH