Other Parts Discussed in Thread: AM3892, MSP430F2132, AM3894
Hello,
I have custom board based on TI AM3892 processor. We've managed to run Linux + Arago FS on board through the agency of E2E Community and espesially Pavel Botev. The board's design is very similar to DM816x/CA816x/AM389x EVM but there are some valuable differences. Now we are trying to run HDMI.
I have a questions about syslink at first:
There is two processors on EVM: cortex A8 and MSP430F2132. On our board we have A8 only. As said in wiki pages syslink library is a funcional layer controlling the inter-processor communction between Cotex A8 and Cotex M3(http://processors.wiki.ti.com/index.php/DM816X_C6A816X_AM389X_VPSS_Video_Driver_User_Guide_PSP_04.00.00.12) (here is misspelling in your wiki page, Cotex instead of Cortex). Since I have only one processor on my board, do I need syslink module to run HDMI?
I tryed to load HDMI related modules without the syslink and I failed. What can be a reason of the issue?
During linux startup there are following error message, also same message we receive when trying to load vpss linux kernel module manually.
BUG: Your driver calls ioremap() on system memory. This leads
to architecturally unpredictable behaviour on ARMv6+, and ioremap()
will fail in the next kernel release. Please fix your driver.
------------[ cut here ]------------
WARNING: at arch/arm/mm/ioremap.c:211 __arm_ioremap_pfn_caller+0x58/0x190()
Modules linked in: vpss(+)
Backtrace:
[<c0049bb8>] (dump_backtrace+0x0/0x110) from [<c0385f2c>] (dump_stack+0x18/0x1c)
r7:00000000 r6:c004d054 r5:c043c621 r4:000000d3
[<c0385f14>] (dump_stack+0x0/0x1c) from [<c006c6cc>] (warn_slowpath_common+0x54/0x6c)
[<c006c678>] (warn_slowpath_common+0x0/0x6c) from [<c006c708>] (warn_slowpath_null+0x24/0x2c)
r9:d5c14000 r8:c04cab18 r7:bf016530 r6:000a0200 r5:00200000
r4:00000000
[<c006c6e4>] (warn_slowpath_null+0x0/0x2c) from [<c004d054>] (__arm_ioremap_pfn_caller+0x58/0x190)
[<c004cffc>] (__arm_ioremap_pfn_caller+0x0/0x190) from [<c004d210>] (__arm_ioremap_caller+0x64/0x6c)
[<c004d1ac>] (__arm_ioremap_caller+0x0/0x6c) from [<c005f0e4>] (omap_ioremap+0x60/0x64)
r6:00000000 r5:00200000 r4:a0200000
[<c005f084>] (omap_ioremap+0x0/0x64) from [<bf016530>] (vps_sbuf_init+0x108/0x1c0 [vpss])
r7:bf00f628 r6:00200000 r5:a0200000 r4:d5dce940
[<bf016428>] (vps_sbuf_init+0x0/0x1c0 [vpss]) from [<bf0000b0>] (vps_probe+0x4c/0x174 [vpss])
r8:c04dfc30 r7:d5e04000 r6:bf00f5c0 r5:c04cab20 r4:c04cab18
[<bf000064>] (vps_probe+0x0/0x174 [vpss]) from [<c01f40bc>] (platform_drv_probe+0x20/0x24)
r7:d5e04000 r6:bf00f12c r5:c04cab20 r4:c04cab20
[<c01f409c>] (platform_drv_probe+0x0/0x24) from [<c01f3028>] (driver_probe_device+0xd0/0x190)
[<c01f2f58>] (driver_probe_device+0x0/0x190) from [<c01f3150>] (__driver_attach+0x68/0x8c)
r7:d5e04000 r6:bf00f12c r5:c04cab54 r4:c04cab20
[<c01f30e8>] (__driver_attach+0x0/0x8c) from [<c01f27d4>] (bus_for_each_dev+0x50/0x84)
r7:d5e04000 r6:bf00f12c r5:c01f30e8 r4:00000000
[<c01f2784>] (bus_for_each_dev+0x0/0x84) from [<c01f2e4c>] (driver_attach+0x20/0x28)
r6:bf00f12c r5:bf00f118 r4:00000000
[<c01f2e2c>] (driver_attach+0x0/0x28) from [<c01f20ac>] (bus_add_driver+0xb4/0x234)
[<c01f1ff8>] (bus_add_driver+0x0/0x234) from [<c01f3488>] (driver_register+0xb0/0x13c)
[<c01f33d8>] (driver_register+0x0/0x13c) from [<c01f43a8>] (platform_driver_register+0x4c/0x60)
r9:d5c14000 r8:bf015000 r7:401e5000 r6:0001b3e0 r5:bf00f118
r4:00000000
[<c01f435c>] (platform_driver_register+0x0/0x60) from [<c01f43dc>] (platform_driver_probe+0x20/0x70)
[<c01f43bc>] (platform_driver_probe+0x0/0x70) from [<bf015030>] (vps_init+0x30/0x5c [vpss])
r5:bf00f49c r4:00000000
[<bf015000>] (vps_init+0x0/0x5c [vpss]) from [<c003b42c>] (do_one_initcall+0xd0/0x1a4)
[<c003b35c>] (do_one_initcall+0x0/0x1a4) from [<c0097de8>] (sys_init_module+0x9c/0x1bc)
[<c0097d4c>] (sys_init_module+0x0/0x1bc) from [<c0045e00>] (ret_fast_syscall+0x0/0x30)
r7:00000080 r6:00000000 r5:0001b3e0 r4:4008abe0
---[ end trace 4e31c9709dc48486 ]---
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
VPSS_CORE : Failed to init fvid2 interface,
vpss: probe of vpss failed with error -22
VPSS_CORE : failed to register ti81xx-vpss driver
Best regards,
Anton