This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCIe and SRIO throughput performance



Hi,

In “Throughput Performance Guide for C66x KeyStone Devices”  all PCIe and SRIO throughput performance are mentioned, and I can say about shannon:

- PCIe: the efficiency is about 128/128+24+8 =80%

- SRIO: the efficiency is about 256/(256+20) =92%

So in my case[communication between Shannons], if I want make a comparison between PCIe and SRIO I observe that SRIO should be more performant than PCIe due to Data payload size  and Overhead considerations!

May I ask there are others considerations that I should take care about in my comparison?

However, it is possible that PCIe can be better than SRIO in some cases ?! 

  • Ahh, the old which is better question :)  It really depends on the application and system connectivity needed.  Let me give you a few things to consider...

    How big is the system (number of endpoints)? SRIO scales well.

    Do you need peer-to-peer communiction? PCIe routes traffic through the RC, while SRIO is direct peer-to-peer

    Are the transactions memory mapped read/writes, or is messaging desired? Both support memory mapped, SRIO additionally supports messaging.

    Do I need address translation? Only PCIe supports within the peripheral.  You could optionally look at system level MPAX registers for translation.

    Bandwidth required? PCIe is 2 lanes 5Gbps, SRIO supports 4 lanes at 5Gbps

    Do you need to connect to an Intel host?  Backplane involved?  PCIe is the way to go for any direct connection to Intel hosts.

    I could probably go on and on, but hopefully that helps you think of some of the other system issues.

    Regards,

    Travis