I am just starting to explore boot load issues seen with a new board design. Other engineers reported bootload from flash not working, but a GEL file with an emulator works. I don't have hardware yet, but another discussion here talks about not using pullup/pulldown resistors on several HD pins. Our schematic shows part number SM32C6713BGDPA20EP. I have a 6713-EP / 6713B-EP data manual (revised April 2011), but is this a 6713-EP part or a 6713B-EP part? (I think the BG stands for ball grid). The schematic shows the following connections:
HD[15, 14, 13, 11, 10, 9, 7, 6, 5, 2, 1, 0] - no connection
HD[12, 8, 4] - pulled up to 3.3v with 10K
HD[3] - ground (no pulldown)
Can you verify these connections are ok and should not affect bootload?
Thanks, John