Other Parts Discussed in Thread: TMS320C6748
Hi,
We have designed a custom board of tms320c6748 and there will be a current problem with 1.8 volt.
When we supply power to board and release from reset then the 1.8 volt of processer will take 500mA current and this wil make a processor heat up.
Other voltages like 3.3 and 1.3 are fine.
We can not use DDR on custom board.
The working of board is fine we connect it to CCS and load a program and the program of blinking led is fine and it will work.
Only problem is the current problem which is due to 1.8volt.
Thanks