Other Parts Discussed in Thread: OMAP-L138, TCA6416, DA8XX, PMP
Hi,
I follow the link in 'Booting Linux kernel using U-Boot' to download arago-base-image-arago.ext2.gz which is under 2009.11 release directory. But the linux kernel failed to mout to file system. It complains about 'FATAL: Could not open /lib/modules/3.3.0+/modules.dep.temp for writing: No such file or directory' and fails to mount to ramdisk / directory.
I tried several different releases like 03-2010 and 05-2010, but they all failed. Anyone has similar problem? Where I can find a working ramdisk? Following is the console output. I can login as root, but no file system available.
U-Boot 2009.11 (May 03 2010 - 15:38:40)
I2C: ready
DRAM: 64 MB
In: serial
Out: serial
Err: serial
ARM Clock : 300000000 Hz
DDR Clock : 132000000 Hz
Net: Ethernet PHY: GENERIC @ 0x00
Hit any key to stop autoboot: 0
8192 KiB M25P64 at 0:0 is now current device
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-3.3.0+
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2553928 Bytes = 2.4 MB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Booting Linux on physical CPU 0
Linux version 3.3.0+ (x0029463@psplinux060) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 PREEMPT Thu Aug 9 21:35:50 IST 2012
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: DaVinci DA850/OMAP-L138/AM18x EVM
Memory policy: ECC disabled, Data cache writeback
BUG: mapping for 0x80000000 at 0xfffe0000 out of vmalloc space
DaVinci da850/omap-l138/am18x variant 0x1
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 8128
Kernel command line: mem=32M console=ttyS2,115200n8 root=/dev/ram0 rw initrd=0xc1180000,4m ip=off
PID hash table entries: 128 (order: -3, 512 bytes)
Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)
Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)
Memory: 32MB = 32MB total
Memory: 22980k/22980k available, 9788k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0xc2800000 - 0xff000000 ( 968 MB)
lowmem : 0xc0000000 - 0xc2000000 ( 32 MB)
modules : 0xbf000000 - 0xc0000000 ( 16 MB)
.text : 0xc0008000 - 0xc04b8000 (4800 kB)
.init : 0xc04b8000 - 0xc04e3000 ( 172 kB)
.data : 0xc04e4000 - 0xc051f3e0 ( 237 kB)
.bss : 0xc051f404 - 0xc053ce8c ( 119 kB)
SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:245
Console: colour dummy device 80x30
Calibrating delay loop... 148.88 BogoMIPS (lpj=744448)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
Setting up static identity map for 0xc0392218 - 0xc0392270
gpiochip_add: registered GPIOs 0 to 31 on device: DaVinci
gpiochip_add: registered GPIOs 32 to 63 on device: DaVinci
gpiochip_add: registered GPIOs 64 to 95 on device: DaVinci
gpiochip_add: registered GPIOs 96 to 127 on device: DaVinci
gpiochip_add: registered GPIOs 128 to 143 on device: DaVinci
DaVinci: 144 gpio irqs
print_constraints: dummy:
NET: Registered protocol family 16
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
print_constraints: VDCDC1: 3200 <--> 3300 mV at 3300 mV
print_constraints: VDCDC2: 1750 <--> 3300 mV at 3300 mV
print_constraints: VDCDC3: 950 <--> 1350 mV at 1200 mV
print_constraints: LDO1: 1800 mV
print_constraints: LDO2: 1150 <--> 1300 mV at 1200 mV
pca953x 1-0020: failed reading register
pca953x 1-0021: interrupt support not compiled in
gpiochip_add: registered GPIOs 160 to 175 on device: tca6416
i2c-gpio i2c-gpio.1: using pins 20 (SDA) and 21 (SCL)
Advanced Linux Sound Architecture Driver Version 1.0.24.
Switching to clocksource timer0_1
musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
musb-hdrc musb-hdrc: dma type: dma-cppi41
MUSB255 controller's USBSS revision = 4ea11003
Waiting for USB PHY clock good...
musb-hdrc musb-hdrc: USB OTG mode controller at fee00000 using DMA, IRQ 58
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 1024 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 1024 bind 1024)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (no cpio magic); looks like an initrd
Freeing initrd memory: 4096K
EMAC: MII PHY configured, RMII PHY will not be functional
JFFS2 version 2.2. (NAND) 2001-2006 Red Hat, Inc.
msgmni has been set to 52
io scheduler noop registered (default)
da8xx_lcdc da8xx_lcdc.0: GLCD: Found Sharp_LK043T1DG01 panel
Console: switching to colour frame buffer device 60x34
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25) is a AR7
serial8250.0: ttyS1 at MMIO 0x1d0c000 (irq = 53) is a AR7
serial8250.0: ttyS2 at MMIO 0x1d0d000 (irq = 61) is a AR7
console [ttyS2] enabled
brd: module loaded
ahci ahci: forcing PORTS_IMPL to 0x1
ahci ahci: AHCI 0001.0100 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci: flags: ncq sntf pm led clo only pmp pio slum part ccc
scsi0 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x01e18000-0x01e19fff] port 0x100 irq 67
spi_davinci spi_davinci.1: DMA: supported
spi_davinci spi_davinci.1: DMA: RX channel: 18, TX channel: 19, event queue: 0
m25p80 spi1.0: m25p64 (8192 Kbytes)
Creating 6 MTD partitions on "m25p80":
0x000000000000-0x000000010000 : "UBL"
0x000000010000-0x000000090000 : "U-Boot"
0x000000090000-0x0000000a0000 : "U-Boot-Env"
0x0000000a0000-0x000000320000 : "Kernel"
0x000000320000-0x000000720000 : "Filesystem"
0x0000007f0000-0x000000800000 : "MAC-Address"
Read MAC addr from SPI Flash: ff:ff:ff:ff:ff:ff
spi_davinci spi_davinci.1: Controller at 0xfef0e000
davinci_mdio davinci_mdio.0: davinci mdio revision 1.5
davinci_mdio davinci_mdio.0: detected phy mask fffffffe
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[0]: device davinci_mdio-0:00, driver SMSC LAN8710/LAN8720
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
ohci ohci.0: DA8xx OHCI
ohci ohci.0: new USB bus registered, assigned bus number 1
Waiting for USB PHY clock good...
ohci ohci.0: irq 59, io mem 0x01e25000
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
input: gpio-keys-polled as /devices/platform/gpio-keys-polled.1/input/input0
input: TPS6507x Touchscreen as /devices/platform/i2c-gpio.1/i2c-1/1-0048/input/input1
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
omap_rtc: RTC power up reset detected
i2c /dev entries driver
lirc_dev: IR Remote Control driver registered, major 253
ata1: SATA link down (SStatus 0 SControl 300)
IR NEC protocol handler initialized
IR RC5(x) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR RC5 (streamzap) protocol handler initialized
IR SANYO protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR LIRC bridge handler initialized
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (1.1.1)
watchdog watchdog: heartbeat 60 sec
cpuidle: using governor ladder
cpuidle: using governor menu
davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usbcore: registered new interface driver snd-usb-audio
soc-audio soc-audio.0: ASoC: Failed to create card debugfs directory
_regulator_get: 1-0018 supply IOVDD not found, using dummy regulator
_regulator_get: 1-0018 supply DVDD not found, using dummy regulator
_regulator_get: 1-0018 supply AVDD not found, using dummy regulator
_regulator_get: 1-0018 supply DRVDD not found, using dummy regulator
asoc: tlv320aic3x-hifi <-> davinci-mcasp.0 mapping ok
ALSA device list:
#0: DA850/OMAP-L138 EVM
TCP cubic registered
NET: Registered protocol family 17
regulator_init_complete: LDO2: incomplete constraints, leaving on
regulator_init_complete: LDO1: incomplete constraints, leaving on
regulator_init_complete: VDCDC3: incomplete constraints, leaving on
regulator_init_complete: VDCDC2: incomplete constraints, leaving on
regulator_init_complete: VDCDC1: incomplete constraints, leaving on
console [netcon0] enabled
netconsole: network logging started
davinci_emac davinci_emac.1: using random MAC addr: 3a:f1:8b:b0:ec:4d
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
RAMDISK: gzip image found at block 0
VFS: Mounted root (ext2 filesystem) on device 1:0.
Freeing init memory: 172K
INIT: version 2.86 booting
Please wait: booting...
Starting udev
udevd (611): /proc/611/oom_adj is deprecated, please use /proc/611/oom_score_adj instead.
Populating dev cache
Remounting root file system...
WARNING: Couldn't open directory /lib/modules/3.3.0+: No such file or directory
FATAL: Could not open /lib/modules/3.3.0+/modules.dep.temp for writing: No such file or directory
modprobe: FATAL: Could not load /lib/modules/3.3.0+/modules.dep: No such file or directory
modprobe: FATAL: Could not load /lib/modules/3.3.0+/modules.dep: No such file or directory
root: mount: mounting rootfs on / failed: No such file or directory
root: mount: mounting usbfs on /proc/bus/usb failed: No such file or directory
Setting up IP spoofing protection: rp_filter.
Configuring network interfaces... davinci_mdio davinci_mdio.0: resetting idled controller
net eth0: attached PHY driver [SMSC LAN8710/LAN8720] (mii_bus:phy_addr=davinci_mdio-0:00, id=7c0f1)
udhcpc (v1.13.2) started
Sending discover...
Sending discover...
Sending discover...
No lease, failing
done.
Fri Dec 11 11:54:00 UTC 2009
INIT: Entering runlevel: 5
Starting telnet daemon.
Starting syslogd/klogd: modprobe: FATAL: Could not load /lib/modules/3.3.0+/modules.dep: No such file or directory
done
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|
Arago Project http://arago-project.org arago ttyS2
Arago 2009.11 arago ttyS2
Thanks,
Tom