Hi,
The link: http://processors.wiki.ti.com/index.php/MCSDK_VIDEO_2.1_PKT_Demo_Guide
talked the MPlayer compatibility problem with Windows 7. I cannot find the MPUI.2008-02-10 on line. I get a newer version MPlayer. After the installation, I find that it can play I previously saved .mpg file. I don't know this tells whether this MPlayer can work in the video demo or not?
The above link also says sv01.out is image file:
Change the Current Directory to the directory (<MCSDK Video Install Dir>\mcsdk_video_2_1_x_x\demos\pkt_xxx_demo\customBuild\tftp) that contains the DSP image sv01.out. Click the Show Dir button to confirm that sv01.out is located in that directory.
I try load to MPlayer, but it cannot show any image at all. sv01.out is not a pure image data, it seems. But it has 21,753 KB in size. I don't know what code/data structure in it. Is there a simple way to test MPlayer works or not for the Video demo in Windows 7?
Thanks,