hi guys
i'm using sil1161 on DM8148 IO expassion board to receive HD video. And i'm running a DVR _RDK capure_display driver, but the display is gray. I have checked the VIP0 port to verify if there is data streams, and it is. I think I should change some sil1161 register configuration, but the datasheet doesn't tell me any useful information about configuring the output dataformat. Do i need to change the register configuration|? if not, what should i do...
Is there any one who have ever used sil1161, i need some help.