hi:
when i run my program using the dm642 board at ccs2.2, i have encountered a problem as follow:
Can't Set Breakpoint: Error 0x00000008/-1076 Error during: Break Point, Cannot set/verify breakpoint at 0x80018798
Breakpoint Manager: An error was encountered attempting to set a breakpoint used
for end of program detection.
Trouble running Target CPU: Error 0x0000000C/-2044 Error during: Register, Break Point, No breakpoint at 0x00000CA0
the program i design is compiled and built well, its only when i run the program and the problem come out
i think it is a internal storage error,but i donot know how to find out it.
Thanks for anyone could help me!!