This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dspbois config file *.tci understanding

there are some config file *.tci in dspbois folder, which document shall i read to understand these files ?

  • Hi,

    Could you be more specific.  Which .tci files are you speaking of?  Which version of DSPBIOS?

    In general, .tci files are configuration scripts that are included by other configuration files (*.tcf).

    Judah

  • hi, Judah

     dspbios version is 5_41_03_17, for the following tci file, how can i understand each line meaning and modify it ? Thanks!

    /*
    * Copyright 2010 by Texas Instruments Incorporated.
    * @(#) DSP/BIOS_Kernel 5,2,5,28 02-10-2010 (cuda-u28)
    */
    /*
    * ======== bios_6748.tci ========
    * This file contains BIOS settings for 6748.
    *
    */

    /*
    * ======== bios.internal.setupMemory6748 ========
    * This function is the top-level function that will remove all MEM segments
    * from the cdb file. It will take your physical memory map from calling
    * getMemoryMap() and create MEM instances in cdb.
    * It will then set sections to the default segment specified and fix up
    * the length and/or base of MEM segments if needed.
    */
    bios.internal.setupMemory6748 = function (prog)
    {
    /*
    * Enable the MAR bits for the entire DDR memory range.
    * (0xC000 0000 - 0xDFFF FFFF)
    */
    prog.module("GBL").C64PLUSCONFIGURE = 1;
    prog.module("GBL").C64PLUSMAR192to223 = 0xffffffff;

    /*
    * BIOS MEM segments will be created from object model memory definitions.
    * Place default code and data sections into specified memory segments.
    */
    bios.initializeMemory(prog, "IRAM", "IRAM");

    var iram = prog.module("MEM").instance("IRAM");
    var l1dsram = prog.module("MEM").instance("L1DSRAM");

    bios.internal.setupCache6748(prog, iram);
    }

    /*
    * ======== bios.internal.setupCache6748 ========
    */
    bios.internal.setupCache6748 = function (prog, iram)
    {
    var cpu = prog.cpu;
    var cache_l1p = prog.module("MEM").instance("CACHE_L1P");
    var l1psram = prog.module("MEM").instance("L1PSRAM");

    cache_l1p.len = 0x0;
    cache_l1p.base = l1psram.base + l1psram.len;

    if (cpu.registers.l1PMode == undefined || cpu.registers.l1PMode == null ||
    cpu.registers.l1PMode == "32k") {
    if (l1psram != undefined) {
    l1psram.destroy();
    }
    cache_l1p.base -= 0x8000;
    cache_l1p.len = 0x8000;
    }
    else {
    if (cpu.registers.l1PMode == "0k") {
    l1psram.len -= 0x0;
    }
    else if (cpu.registers.l1PMode == "4k") {
    l1psram.len -= 0x1000;
    }
    else if (cpu.registers.l1PMode == "8k") {
    l1psram.len -= 0x2000;
    }
    else if (cpu.registers.l1PMode == "16k") {
    l1psram.len -= 0x4000;
    }
    else {
    throw new Error("Can't set L1P cache to size: " +
    cpu.registers.l1PMode);
    }
    }

    var cache_l1d = prog.module("MEM").instance("CACHE_L1D");
    var l1dsram = prog.module("MEM").instance("L1DSRAM");
    cache_l1d.len = 0x0;
    cache_l1d.base = l1dsram.base + l1dsram.len;

    if (cpu.registers.l1DMode == undefined || cpu.registers.l1DMode == null ||
    cpu.registers.l1DMode == "32k") {
    if (l1dsram != undefined) {
    l1dsram.destroy();
    }
    cache_l1d.base -= 0x8000;
    cache_l1d.len = 0x8000;
    }
    else {
    if (cpu.registers.l1DMode == "0k") {
    l1dsram.len -= 0x0;
    }
    else if (cpu.registers.l1DMode == "4k") {
    l1dsram.len -= 0x1000;
    }
    else if (cpu.registers.l1DMode == "8k") {
    l1dsram.len -= 0x2000;
    }
    else if (cpu.registers.l1DMode == "16k") {
    l1dsram.len -= 0x4000;
    }
    else throw new Error("Can't set L1D cache to size: " +
    cpu.registers.l1DMode);
    }

    var cache = prog.module("MEM").instance("CACHE_L2");

    cache.len = 0x0;
    cache.base = iram.base + iram.len;

    if (cpu.registers.l2Mode != null) {
    if (cpu.registers.l2Mode == "0k") {
    iram.len -= 0x0;
    }
    else if (cpu.registers.l2Mode == "32k") {
    iram.len -= 0x8000;
    }
    else if (cpu.registers.l2Mode == "64k") {
    iram.len -= 0x10000;
    }
    else if (cpu.registers.l2Mode == "128k") {
    iram.len -= 0x20000;
    }
    else if (cpu.registers.l2Mode == "256k") {
    iram.len -= 0x40000;
    /*
    * All references to IRAM need to be changed to point to some other
    * available MEM instance.
    */
    var memInst = prog.module("MEM").instances();
    var seg = null;
    for (var i=0; i < memInst.length; i++) {
    if (memInst[i].space == "code/data" && memInst[i] != iram) {
    seg = memInst[i];
    }
    }
    if (seg == null) {
    throw new Error("All of IRAM is used for cache " +
    "and there is no external memory in the configuration");
    }
    else {
    bios.setMemCodeSections(prog, seg);
    bios.setMemDataNoHeapSections(prog, seg);
    }
    iram.destroy();
    }
    else {
    throw new Error("Can't set cache to size: " + cpu.registers.l2Mode);
    }
    }
    }

    /*
    * ======== bios.init6748 ========
    * BIOS initialization for the 6748
    */
    bios.init6748 = function (prog, baseseed)
    {
    /*
    * Find configuration seed files to load
    */
    if (baseseed == null) {
    baseseed = "ti/bios/config/cdb/c6748.cdb";
    }

    var seed = utils.findSeed(baseseed);
    if (seed != null) {
    try {
    prog.load(seed);
    }
    catch (e) {
    throw new Error ("Can't load configuration seed '" + seed + "' : "
    + e);
    }
    }
    else {
    throw new Error ("Can't find configuration seed: " + baseseed);

    }

    prog.module("ISRC").instance("Timer_0").iIntrSelectNum = 4;
    prog.module("ISRC").instance("Timer_1").iIntrSelectNum = 40;
    prog.module("HWI").instance("HWI_INT14").interruptSelectNumber = 4;
    prog.module("CLK").TIMER0BASE = 0x01c20000;
    prog.module("CLK").TIMER1BASE = 0x01c21000;
    prog.module("CLK").TIMERSELECT = "Timer 2";

    /* enable specification of Input Clock Rate */
    prog.module("CLK").SPECIFYRATE = true;
    prog.module("CLK").INPUTCLK = 24.0;
    prog.module("CLK").RESETTIMER = true;

    /* set CLKOUT to be the value of cpu.clockRate. */
    bios.internal.setClkout(prog);

    /* Set endian mode based on build options */
    if (prog.build.target.model.endian != null) {
    if (prog.build.target.model.endian != "little") {
    print("Warning: '" + prog.build.target.model.endian +
    "' endian mode" + " is not supported on '" +
    prog.cpu.deviceName + "' device.")
    }
    }

    prog.module("GBL").ENDIANMODE = prog.build.target.model.endian;

    /* initialize the default memory segments for 6748 */
    bios.internal.setupMemory6748(prog);

    /* initialize some memory map registers */
    bios.internal.initializeRegisterMap(prog);
    }

  • Huang,

    These are internal files that are loaded by BIOS and should not be modified.

    In your .tcf file, when you do a utils.loadPlatform(), Based upon the platform you select, BIOS will determine which bios_<device>.tci to load.

    Is there a specific question that you have?

    Judah

  • hi, Judah

    because i want to change bios source clock, i need to modify tci file, see the post

    http://e2e.ti.com/support/embedded/bios/f/355/p/255551/895863.aspx#895863

    thanks!

  • Huang,

    I understand that you want to change the source clock, but you should not modify these internal file to change the source clock.  You should modify your .tcf file or your own .tci file.  These files will simply give you a default configuration which you can change in your .tcf file.

    Judah

  • Hi,Judah

    i only find tic file, I am using c6run, and don't know where to find tcf file

  • Huang,

    Do you not have a .tcf file as part of your project?  Its the configuration file for your BIOS app.

    Judah

  • hi, Judah

    i found "C6Run.tcf" which i think is the tcf file, and it import tci file "utils.importFile("platform.tci");"

    i guess that platform.tci points to the tci file i found before, is it ?

  • Is there a statment that says "utils.loadPlatform" somwhere in your .tcf or an imported .tci file?  That is the one that would eventually load the bios_xxx.tci file.

    Judah

  • hi, Judah

    i find the file, thanks!