Other Parts Discussed in Thread: DA8XX, TPS65910
I change uImage which is unzipped from 335xevm_sk.tar.gz , the borad-am335x.c has been modified as follow:
static struct omap2_hsmmc_info am335x_mmc[] __initdata = {
{
.mmc = 1,
.caps = MMC_CAP_4_BIT_DATA,
.gpio_cd = GPIO_TO_PIN(1, 12),
.gpio_wp = /*GPIO_TO_PIN(1,13)*/-EINVAL,
.ocr_mask = MMC_VDD_32_33 | MMC_VDD_33_34, /* 3V3 */
},
{
.mmc = 0, /* will be set at runtime */
},
But it cant boot up from SD card. I was puzzled that it is ok in kernal 3.1. So what do you think ?
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.2.0 (root@ubuntu) (gcc version 4.4.3 (GCC) ) #24 Mon Apr 1 01:52:43 PDT 2013
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES1.0 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024
[ 0.000000] Kernel command line: console=ttyO0,115200n8 androidboot.console=ttyO0 mem=256M root=/dev/mmcblk0p2 rw rootfstype=ext4 rootwait init=/init ip=off
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 256MB = 256MB total
[ 0.000000] Memory: 251540k/251540k available, 10604k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc065f000 (6492 kB)
[ 0.000000] .init : 0xc065f000 - 0xc0698000 ( 228 kB)
[ 0.000000] .data : 0xc0698000 - 0xc06eebe0 ( 347 kB)
[ 0.000000] .bss : 0xc06eec04 - 0xc081e408 (1215 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000152] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[ 0.058929] pid_max: default: 32768 minimum: 301
[ 0.059051] Security Framework initialized
[ 0.059112] Mount-cache hash table entries: 512
[ 0.059509] CPU: Testing write buffer coherency: ok
[ 0.079437] omap_hwmod: gfx: failed to hardreset
[ 0.095703] omap_hwmod: pruss: failed to hardreset
[ 0.096466] print_constraints: dummy:
[ 0.096710] NET: Registered protocol family 16
[ 0.097778] OMAP GPIO hardware version 0.1
[ 0.098815] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.100433] _omap_mux_get_by_name: Could not find signal gpmc_ad14.gpio1_14
[ 0.100463] _omap_mux_get_by_name: Could not find signal gpmc_ad15.gpio1_15
[ 0.100616] da8xx_lcdc.0: alias fck already exists
[ 0.100799] omap_hsmmc.0: alias fck already exists
[ 0.100952] davinci-mcasp.0: alias fck already exists
[ 0.101074] TSC connected to beta GP EVM
[ 0.101257] d_can.1: alias fck already exists
[ 0.101379] d_can.0: alias fck already exists
[ 0.101531] _omap_mux_get_by_name: Could not find signal gpmc_ad10.gpio0_26
[ 0.102081] omap_i2c.1: alias fck already exists
[ 0.102569] omap2_mcspi.1: alias fck already exists
[ 0.102691] omap2_mcspi.2: alias fck already exists
[ 0.102844] edma.0: alias fck already exists
[ 0.102874] edma.0: alias fck already exists
[ 0.102905] edma.0: alias fck already exists
[ 0.111907] bio: create slab <bio-0> at 0
[ 0.112915] SCSI subsystem initialized
[ 0.113769] usbcore: registered new interface driver usbfs
[ 0.113891] usbcore: registered new interface driver hub
[ 0.114044] usbcore: registered new device driver usb
[ 0.114196] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[ 0.114349] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[ 0.128997] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[ 0.130249] tps65910 1-002d: JTAGREVNUM 0x0
[ 0.132446] print_constraints: VRTC:
[ 0.133789] print_constraints: VIO: at 1800 mV
[ 0.136016] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal
[ 0.138244] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal
[ 0.139160] print_constraints: VDD3: 5000 mV
[ 0.140472] print_constraints: VDIG1: at 1800 mV
[ 0.141815] print_constraints: VDIG2: at 1800 mV
[ 0.143127] print_constraints: VPLL: at 1800 mV
[ 0.144439] print_constraints: VDAC: at 1800 mV
[ 0.145782] print_constraints: VAUX1: at 1800 mV
[ 0.147094] print_constraints: VAUX2: at 3300 mV
[ 0.148437] print_constraints: VAUX33: at 3300 mV
[ 0.149749] print_constraints: VMMC: at 3300 mV
[ 0.150054] tps65910 1-002d: No interrupt support, no core IRQ
[ 0.150543] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.151123] Bluetooth: Core ver 2.16
[ 0.151184] NET: Registered protocol family 31
[ 0.151184] Bluetooth: HCI device and connection manager initialized
[ 0.151214] Bluetooth: HCI socket layer initialized
[ 0.151214] Bluetooth: L2CAP socket layer initialized
[ 0.151275] Bluetooth: SCO socket layer initialized
[ 0.151458] Switching to clocksource gp timer
[ 0.159088] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.159301] musb-hdrc musb-hdrc.0: dma type: pio
[ 0.159912] musb-hdrc musb-hdrc.0: USB OTG mode controller at d081c000 using PIO, IRQ 18
[ 0.160156] musb-hdrc musb-hdrc.1: dma type: pio
[ 0.160400] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.160461] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[ 0.160614] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.160614] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.160644] usb usb1: Product: MUSB HDRC host driver
[ 0.160644] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd
[ 0.160644] usb usb1: SerialNumber: musb-hdrc.1
[ 0.161163] hub 1-0:1.0: USB hub found
[ 0.161163] hub 1-0:1.0: 1 port detected
[ 0.161651] musb-hdrc musb-hdrc.1: USB Host mode controller at d081e800 using PIO, IRQ 19
[ 0.161987] NET: Registered protocol family 2
[ 0.162200] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.162567] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.162719] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.162811] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.162841] TCP reno registered
[ 0.162841] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.162872] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.163085] NET: Registered protocol family 1
[ 0.163360] RPC: Registered named UNIX socket transport module.
[ 0.163360] RPC: Registered udp transport module.
[ 0.163391] RPC: Registered tcp transport module.
[ 0.163391] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.163635] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.163848] omap-gpmc omap-gpmc: GPMC revision 6.0
[ 0.163879] Registering NAND on CS0
[ 0.290283] ashmem: initialized
[ 0.290557] VFS: Disk quotas dquot_6.5.2
[ 0.290618] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.291503] msgmni has been set to 491
[ 0.292541] io scheduler noop registered
[ 0.292572] io scheduler deadline registered
[ 0.292633] io scheduler cfq registered (default)
[ 0.293273] Could not set LED4 to fully on
[ 0.294097] da8xx_lcdc da8xx_lcdc.0: GLCD: Found QY_LCD panel
[ 0.303924] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 1.013183] console [ttyO0] enabled
[ 1.017242] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 1.024932] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 1.032592] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 1.040252] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 1.048065] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 1.061676] brd: module loaded
[ 1.067901] loop: module loaded
[ 1.071380] i2c-core: driver [tsl2550] using legacy suspend method
[ 1.077880] i2c-core: driver [tsl2550] using legacy resume method
[ 1.085205] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.092254] omap2-nand driver initializing
[ 1.096618] pdata->ecc_opt is 4
[ 1.100250] NAND device: Manufacturer ID: 0xec, Chip ID: 0xd3 (Samsung NAND 1GiB 3,3V 8-bit)
[ 1.109649] Creating 8 MTD partitions on "omap2-nand.0":
[ 1.115234] 0x000000000000-0x000000020000 : "SPL"
[ 1.121154] 0x000000020000-0x000000040000 : "SPL.backup1"
[ 1.127746] 0x000000040000-0x000000060000 : "SPL.backup2"
[ 1.134246] 0x000000060000-0x000000080000 : "SPL.backup3"
[ 1.140686] 0x000000080000-0x000000260000 : "U-Boot"
[ 1.147460] 0x000000260000-0x000000280000 : "U-Boot Env"
[ 1.153839] 0x000000280000-0x000000780000 : "Kernel"
[ 1.161865] 0x000000780000-0x000040000000 : "File System"
[ 1.592559] OneNAND driver initializing
[ 1.597167] CAN device driver interface
[ 1.601165] CAN bus driver for Bosch D_CAN controller 1.0
[ 1.607543] d_can d_can.1: device registered (irq=55, irq_obj=56)
[ 1.614471] d_can d_can.0: device registered (irq=52, irq_obj=53)
[ 1.662109] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[ 1.668579] davinci_mdio davinci_mdio.0: detected phy mask fffffff8
[ 1.676910] davinci_mdio.0: probed
[ 1.680480] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
[ 1.687866] davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
[ 1.695220] davinci_mdio davinci_mdio.0: phy[2]: device 0:02, driver unknown
[ 1.702667] PPP generic driver version 2.4.2
[ 1.707305] PPP BSD Compression module registered
[ 1.712219] PPP Deflate Compression module registered
[ 1.717620] usbcore: registered new interface driver cdc_ether
[ 1.723785] usbcore: registered new interface driver cdc_eem
[ 1.729736] usbcore: registered new interface driver dm9601
[ 1.735595] usbcore: registered new interface driver cdc_subset
[ 1.741821] cdc_ncm: 04-Aug-2011
[ 1.745269] usbcore: registered new interface driver cdc_ncm
[ 1.751251] usbcore: registered new interface driver cdc_acm
[ 1.757141] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[ 1.765502] Initializing USB Mass Storage driver...
[ 1.770721] usbcore: registered new interface driver usb-storage
[ 1.777008] USB Mass Storage support registered.
[ 1.781982] usbcore: registered new interface driver usbserial
[ 1.788116] USB Serial support registered for generic
[ 1.793457] usbcore: registered new interface driver usbserial_generic
[ 1.800262] usbserial: USB Serial Driver core
[ 1.804870] USB Serial support registered for opticon
[ 1.810180] usbcore: registered new interface driver opticon
[ 1.816162] USB Serial support registered for GSM modem (1-port)
[ 1.822570] usbcore: registered new interface driver option
[ 1.828369] option: v0.7.2:USB Driver for GSM modems
[ 1.835327] gadget: Mass Storage Function, version: 2009/09/11
[ 1.841491] gadget: Number of LUNs=1
[ 1.845367] lun0: LUN: removable file: (no medium)
[ 1.850677] gadget: android_usb ready
[ 1.854644] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 1.860229] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2
[ 1.868072] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 1.875183] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 1.882720] usb usb2: Product: MUSB HDRC host driver
[ 1.887878] usb usb2: Manufacturer: Linux 3.2.0 musb-hcd
[ 1.893432] usb usb2: SerialNumber: musb-hdrc.0
[ 1.898651] hub 2-0:1.0: USB hub found
[ 1.902587] hub 2-0:1.0: 1 port detected
[ 1.907287] mousedev: PS/2 mouse device common for all mice
[ 1.913970] input: ti-tsc-adcc as /devices/platform/omap/tsc/input/input0
[ 1.922485] using rtc device, omap_rtc, for alarms
[ 1.927337] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
[ 1.934234] i2c /dev entries driver
[ 1.938079] Linux video capture interface: v2.00
[ 1.943054] usbcore: registered new interface driver uvcvideo
[ 1.949035] USB Video Class driver (1.1.1)
[ 1.955108] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.961608] device-mapper: uevent: version 1.0.3
[ 1.966674] device-mapper: ioctl: 4.22.0-ioctl (2011-10-19) initialised: dm-devel@redhat.com
[ 1.975494] Bluetooth: HCI UART driver ver 2.2
[ 1.980133] Bluetooth: HCI H4 protocol initialized
[ 1.985137] Bluetooth: HCILL protocol initialized
[ 1.990020] Bluetooth: Bluetooth Driver for TI WiLink - Version 1.0
[ 1.998382] cpuidle: using governor ladder
[ 2.002838] cpuidle: using governor menu
[ 2.009063] usbcore: registered new interface driver usbhid
[ 2.014923] usbhid: USB HID core driver
[ 2.019439] logger: created 256K log 'log_main'
[ 2.024291] logger: created 256K log 'log_events'
[ 2.029296] logger: created 256K log 'log_radio'
[ 2.034240] logger: created 256K log 'log_system'
[ 2.039672] usbcore: registered new interface driver snd-usb-audio
[ 2.047180] _regulator_get: 1-0018 supply IOVDD not found, using dummy regulator
[ 2.054992] _regulator_get: 1-0018 supply DVDD not found, using dummy regulator
[ 2.062683] _regulator_get: 1-0018 supply AVDD not found, using dummy regulator
[ 2.070343] _regulator_get: 1-0018 supply DRVDD not found, using dummy regulator
[ 2.081329] asoc: tlv320aic3x-hifi <-> davinci-mcasp.0 mapping ok
[ 2.088531] ALSA device list:
[ 2.091613] #0: AM335X EVM
[ 2.094665] oprofile: hardware counters not available
[ 2.099914] oprofile: using timer interrupt.
[ 2.104583] nf_conntrack version 0.5.0 (3930 buckets, 15720 max)
[ 2.111267] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 2.117004] TCP cubic registered
[ 2.120513] NET: Registered protocol family 10
[ 2.125885] IPv6 over IPv4 tunneling driver
[ 2.130889] NET: Registered protocol family 17
[ 2.135589] can: controller area network core (rev 20090105 abi 8)
[ 2.142150] NET: Registered protocol family 29
[ 2.146850] can: raw protocol (rev 20090105)
[ 2.151306] can: broadcast manager protocol (rev 20090105 t)
[ 2.157409] Bluetooth: RFCOMM TTY layer initialized
[ 2.162597] Bluetooth: RFCOMM socket layer initialized
[ 2.167938] Bluetooth: RFCOMM ver 1.11
[ 2.171844] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 2.177398] Bluetooth: BNEP filters: protocol multicast
[ 2.182861] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 2.189178] Registering the dns_resolver key type
[ 2.194152] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 2.202178] ThumbEE CPU extension supported.
[ 2.206695] mux: Failed to setup hwmod io irq -22
[ 2.212310] Power Management for AM33XX family
[ 2.217163] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[ 2.223815] Copied the M3 firmware to UMEM
[ 2.228118] omap_hwmod: wkup_m3: wkup_m3: hwmod data error: OMAP4 does not support st_shift
[ 2.240753] clock: disabling unused clocks to save power
[ 2.247802] Detected MACID=0:17:ea:9d:73:f3
[ 2.253387] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:01 UTC (946684801)
[ 2.262695] Waiting for root device /dev/mmcblk0p2...
[ 2.303161] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 2.314117] mmc0: new high speed SDHC card at address 1234
[ 2.320343] mmcblk0: mmc0:1234 SA04G 3.63 GiB