This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need help for buidroot

Hi everybody.

I've AM335x Evaluation Module board from TI.

I have problem when I use builroot to build file system.

It was hangs after network started like this link http://buildroot.uclibc.org/downloads/manual/manual.html#faq-boot-hang-after-starting.

please tell me how can I add ttyO0 driver when I use buildroot ?

Or any way to use buildroot for this board.

  • Hi,

    I believe the answer to your problem is inside the link you posted:

    In order to have the system start a shell on your serial console, you have to go into the Buildroot configuration, System configuration, and modify Port to run a getty (login prompt) on and Baudrate to use as appropriate. This will automatically tune the /etc/inittab file of the generated system so that a shell starts on the correct serial port.

    Best regards,
    Miroslav

  • Miroslav Kiradzhiyski XID said:

    Hi,

    I believe the answer to your problem is inside the link you posted:

    In order to have the system start a shell on your serial console, you have to go into the Buildroot configuration, System configuration, and modify Port to run a getty (login prompt) on and Baudrate to use as appropriate. This will automatically tune the /etc/inittab file of the generated system so that a shell starts on the correct serial port.

    Best regards,
    Miroslav

    [/quote]

    hi Miroslav

        In system configuration I was change port to TTYO0 when it start up It shown

            can't open /dev/ttyO0: No such file or directory

     

     

  • Hi,

    Which kernel version are you using? Are you using the officially supported TI AM335x SDK/PSP? Which SDK/PSP version?

    Please post your .config file (located in the main kernel source code folder), your /etc/inittab (located in your root file system), and finally print your U-Boot bootargs (while in U-Boot mode use this command: print) and post them here.

    Best regards,
    Miroslav

  • Hi

          Thank you for your kindly.At the first time I use u-boot,kernel (linux-3.2.0,psp05.06.00.00 ) and Arago's file system that provided by TI.

    It's works correctly.But that file system not have utilities which I want to use such as ftpserver,nano editor.

    So I use buildroot to building file system and then have that problem.

         configuration and other files I'll attach tomorrow.

    Best Regards

  • Hi,

    What about the other information:

    Miroslav Kiradzhiyski XID said:
    Please post your .config file (located in the main kernel source code folder), your /etc/inittab (located in your root file system), and finally print your U-Boot bootargs (while in U-Boot mode use this command: print) and post them here.

    Best regards,
    Miroslav

  • Miroslav

        I've attached files below.Please read 'ReadMe1st'.

    1256.File4E2E.tar.gz

    Best Regards,

    Peerapong

  • Now this problem has been solved by enable "Maintain a devtmpfs to mount at /dev" in Device Drivers>Generic Driver Options  in kernel configuration