Hi,
I have a 6678EVM board , AMC-PCIe adapter card and DM8168EVM board, TI provide ubuntu desktop-linux-sdk and mcsdk_video_xxx package based on the the pc machine, which can achieve the communication between pc machine and 6678 through AMC-PCIe adapter card .Now, I want to use 8168EVM board instead of a PC to execute ./init_dsp.sh and the other operation on 8168.
1.Can it possible to achieve?
2.If it can achieve, how to cross-compile desktop-linux-sdk correctly?
3.If it can not be achieved, is there any other examples can achieve transfer image files from 8168PCIe to 6678 and let 6678 run?