Other Parts Discussed in Thread: TPS65217
Hi,
when I do a hot plug with my board which based on beaglebone,the board entrys an error state,it doesn't work any more.
Normally,doing a hot-plug means a power-on reset,and the board works OK.
But,sometimes,the board boots failed,it is reseted by the external watchdog ,I disable the internal watchdog,and using an external watchdog.
I found that the supply of TPS65217 is OK(3V3A,3V3B,and so on).
I use a XDS100v2 connect the CPU througth the JTAG interface, it successed.
control_status Register ,0x44e10040,value is 0x00400300,SYSBOOT:0x4000,it is error.
what‘s wrong?
YanTCK