This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

maximum bit-rate

Guru 20755 points

Hello,

Trying to change H.264 codec bit rate above 22Mbit/sec I receive the following messages, while in the user's guide FAQ section it is said that maximum allowed bit rate is 50Mbit/sec. Why do we receive this error message and does it mean the maximum bit-rate is different than the one mentioned.

Regards,

Ran

 [m3video] 1088648:!ERROR!:ENCLINK::links_m3video/iva_enc/encLink_h264.c:[232]::INTERNAL ERROR:-1
 [m3video] ALGCONTROL FAILED:CMD:1
 [m3video] ERROR: IH264ENC_LEVEL_INCOMPLAINT_PARAMETER , 0,  
 [m3video] 1088648:WARN
 [m3video]  ENCLINK: ERROR in Run time parameters changes, Extended Error code:1