Hi, everyone
I'm use beagleboard-xm DM3730 to develop android 2.3.4 (rowboat-gingerbread-dsp). Now I want to use USB camera. I found the UVC in the kernel(2.6.37).Unfortunately,three USB cameras could only one to be identified . Console print UVC found a USB camera as input.But when i start camera app which the system build in, the app terminated. I download some camera app to run,the are also work incorrectly.other two Logitech USB camera couldn't suport,just found USB id.
So, i want to know , if i want to use the USB camera on rowboat android 2.3.4 with dsp, how to do it? if there were any guides?