This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5515 EVM AND CCS V5 PROGRAMMING ISSUE

Hi !

I am new to ccs 5 and c5515. I got c5515 evm from ti.  Evm kit and sample code are working good.but when  i try  to build and generate the .out file, i got the following error :


**** Build of configuration Debug for project first ****

"C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all
'Building file: ../main.c'
'Invoking: C5500 Compiler'
"C:/ti/ccsv5/tools/compiler/c5500_4.4.1/bin/cl55" -v5515 --memory_model=huge -O0 -g --include_path="C:/ti/ccsv5/tools/compiler/c5500_4.4.1/include" --define=c5515 --display_error_number --diag_warning=225 --ptrdiff_size=32 --preproc_with_compile --preproc_dependency="main.pp" "../main.c"
'Finished building: ../main.c'
' '
'Building target: first.out'
'Invoking: C5500 Linker'
"C:/ti/ccsv5/tools/compiler/c5500_4.4.1/bin/cl55" -v5515 --memory_model=huge -g --define=c5515 --display_error_number --diag_warning=225 --ptrdiff_size=16 -z -m"first.map" --stack_size=0x200 --heap_size=0x400 -i"C:/ti/ccsv5/tools/compiler/c5500_4.4.1/lib" -i"C:/ti/ccsv5/tools/compiler/c5500_4.4.1/include" --reread_libs --display_error_number --warn_sections --rom_model --sys_stacksize=0x200 -o "first.out" "./main.obj" -l"libc.a" "../C5515.cmd"
>> ERROR: Only --ptrdiff_size=32 is allowed for huge memory model
gmake: *** [first.out] Error 1
gmake: Target `all' not remade because of errors.

**** Build Finished ****

 pls help me to solve this error!

thanks in advance!