Hi,
I am trying to boot Blaze board using Android Jelly bean 4AJ.2.2 using SD card. I followed the instructions given in http://www.omappedia.com/wiki/4AJ.2.2_OMAP4_Jelly_Bean_Release_Notes and was successful in building the x-loader, u-boot, kernel and the android file system.
I followed 2 methods to flash the sd card.
Method 1:
Followed the instructions given in the release notes (i.e to use fastboot)
Method 2:
Manually copied MLO u-boot and kernel to the boot partition and android file system to the rootfs partition.
After making the appropriate switch settings and booting the board using SD card, android comes up on Blaze display for a brief time but it freezes and i cannot access the board touchscreen.
I have attached the log for your reference.
Any help would be greatly appreciated.
Thanks
Prakash