Hi,
We are trying to define the best PinMux for our board.
Following peripherals need to be used (at the same time for sure):
1) Memory Access
DDR3
NOR Flash 16 bits parallel: 512MB
SRAM 16bits parallel: 4MB
NAND Flash MMC 8 bits
SD card MMC 4 bits
2) External Communication
1 x Ethernet 10/100
1 x CAN
1 x USB Device
1 x USB Host
2 x UART Tx/Rx
1 x UART Tx/Rs + RTS/CTS
1 optional x UART Tx/Rs + RTS/CTS
3) Internal Communication
2 x I2C
1 x SPI
Attached the best PinMux we have been able to get, but we still have some conflicts.
A) High GPMC address conflict with MMC bus
B) Only one I2C available out of the 2 expected
C) We can't have the fourth optional UART
Could anyone help us in order the AM335x fit our requirements or indicate other TI part that should fit ?
Thanks for your support,
Pousse