This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM365

Other Parts Discussed in Thread: TMS320DM365

Hi All,

We are planning to interface Image sensor (OV7955) to TMS320DM365.

Image sensor has to be configured using SCCB (Serial Camera Contoll Bus) interface from master.

Can I connct SCCB interface lines to I2C lines of TMS320DM365.?

Thanks

  • Mohana,

    SCCB and I2C are same. Please use the same lines as I2C. 

  • 3124.dm365.pdfHello,

    I have one more question w.r.t RTC.The intension of using PRTCSS is to retain the time. We are not using PRTCSS for power sequencing.RTC module has back-up supply during power failure.

    • When the RTC module is enabled , it always in loop saying that Busy bit=1
    • We have missed to bring PWCTRIOx pins out, hence we don’t have any provisions to connect the PWCTRI0 pin to low
    • w.r.t attached schematics: R220 & R219 are not mounted in the board.PWCTRO0 is always “0”
      and it resets the board if we mount R220
    • Prototype board is  working fine other than RTC

    Can we do any work around to overcome from the Busy state & retain the RTC value during Reset?

    Thanks,

    Mohan